Functional modules for press automation

press automation 1181x353

 

6 axis robots specially designed for press automation. 7 axis robots for faster transfer, as the parts are not rotated between presses. Two families of 7-axis robots, related with the motion type of the 7th axis:

  • The rotational 7th axis solution combines rotational movements to maintain the part orientation between presses.
  • The linear 7th axis offers the additional advantage of a compound linear acceleration while moving in and out of the press.

Twin robot For high speed press automation, with two manipulators (only one controller) for is an optimum distribution of higher power.

 

Our portfolio

 

Discover more

 

Select region / language