Production manager
Production manager monitors and controls the production cycle, is application independent and can also be used in non-welding applications.
Production Manager is a standardized cell control software which takes care of the following tasks in a robot cell:
- Describe your parts to produce
- Run Setup and Service routines at certain intervals
- Map our physical cell layout to logical work areas
- Organize program flow in a standardized chain of events, maintaining dynamic execution
- Synchronize certain jobs if MultiMove
- Initiate the production via PLC or an Operator