ABB integrates position control in ACS880 drives for cost-effective simplicity

ABB integrates position control in ACS880 drives for cost-effective simplicity

Embedded position control in ABB: ACS880 variable speed drives will reduce costs and simplify machine building

ABB is integrating positioning control within its ACS880 variable speed drives to allow operators to meet motion system demands without the need of an external controller. Embedding position control inside the drive minimizes machine engineering and installation work, removes the need for additional equipment and lowers costs.

Traditionaly, separate devices are used for position control and speed and torque. Position control is implemented using a motion controller with specific tools, user interfaces and programming languages. The power range of these separate controllers are typically limited to under 20 kilowatts (kW) depending on the manufacturer.

The ACS880 with embedded position control offers an alternative solution and a power range up to 5600 kW. It features several pre-programmed functions, including homing modes, absolute and relative positioning, profiled positioning, position synchronizing and fast position latching. The ACS880 also offers encoderless position capabilities and regenerative solutions.

The motion functions are available through a simple parameter interface. Modification and extension of the functions are done by common IEC61131 programming using PLC Open motion blocks. The ACS880 supports almost any type of motor, feedback device and communication protocol.

The ACS880 drives are suitable for a variety of applications and engineered to perform in harsh environments. “These drives have been successfully tested in numerous motion control applications, including stacker cranes, metal presses, sorting and packaging lines, rotary tables and cutting systems,” said Tuomo Tarula, Global Product Management Manager, Drives, ABB. “These tests have proven the drives’ high performance and flexibility.”

The ACS880 platform enables the same product family to be used across the whole production line regardless of whether there is a need for positioning, speed or torque control. This means less training, tools and spare parts are required.

Programming flexibility, together with connectivity to all motors and PLCs, ensure ACS880 is the optimal solution for various applications from stacker cranes, metal presses, sorting and packaging lines, rotary tables to cutting systems.
Programming flexibility, together with connectivity to all motors and PLCs, ensure ACS880 is the optimal solution for various applications from stacker cranes, metal presses, sorting and packaging lines, rotary tables to cutting systems.

ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in power grids, electrification products, industrial automation and robotics and motion, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner in ABB Formula E, the fully electric international FIA motorsport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 147,000 employees. www.abb.com

Links

Kontaktieren Sie uns

Downloads

Diesen Artikel teilen

Facebook LinkedIn Twitter WhatsApp