Electrification Business

Become an ABB AC Wallbox approved installer and claim back up to £350* from OZEV

EV Image
This is to register to install our products, as part of the OZEV (Office for Zero Emission Vehicles) government grant scheme

What is needed to become an approved installer

You "the installer" will need to register with OZEV as an approved installer, You will also need a letter from us stating that you are approved to install our products, which we will provide upon successful completion of our application process.

The OZEV EV charger grant schemes

The Electric Vehicle Home-charge Scheme (EVHS)* provides grant funding of up to 75% (maximum of £350) towards the cost of installing and supplying electric vehicle charge-points at domestic properties throughout England, perfect for electric car charging at home.


The Workplace Charging Scheme (WCS) is similar but the end user business can claim for up to 40 sockets at a maximum of £350 each.

*As of 1st September 2020, the installer only needs to be approved by the manufacturer under the WCS scheme. For EVHS installations, manufacturer’s approval is no longer required.

In line with OZEV requirements all ABB Terra AC Wallboxes come with a 3 year warranty

To claim the grant, the following three conditions must be met:

*Under the EV Homecharge Scheme (EVHS), a claim can be made for up to two chargers (as long as you have two registered EVs) and under the Workplace Charging Scheme (WCS), it is up to £350 per socket for up to 40 sockets.
Select region / language