Field Information Manager supports the user when working with touchscreen devices. Several controls will appear in a design more suitable for touchscreen devices when the Enhanced Touch Mode is enabled via the "hand" icon.
Enable this option if you are using a touch device (like a tablet). Usually the Enhanced Touch Mode reshapes several controls of the user interface to display them with more free space in between.
Please note that the Enhanced Touch Mode disables the standard mouse behavior for accessing the tooltips. For displaying the tooltips, it's required to use the Tooltip Picker then.
Click on the Enhanced Touch Mode button in the top right corner of Field Information Manager to activate or deactivate this mode.