The mapping of Common Names for one or more Device Packages can be exported and imported via the Device Catalog.
The export functionality is available in the context menu of selected Device Packages. The user can configure the export settings, e.g. by selecting Namespaces for export. All required information regarding Common Names of a selected Device Package and Namespace is exported to a CSV file. Besides information about the Device Package, Namespace and available Common Names, the exported file contains the complete Device Package item structure. The column "Common Name" either displays the already assigned Common Name or provides the option to enter one.
For an easy identification of Device Package items, the user can specify that example values shall be included in the exported file. These example values are read from the first online device using this Device Package.
The CSV file serves two purposes:
- It stores all existing mapping information of Common Names to specific Device Package items.
- It allows user-friendly manual mapping in standard text editors or even easier in Microsoft Excel. Within Microsoft Excel, the list of available Common Names can be configured as input for a dropdown menu. This ensures an efficient mapping process of the required Common Name to a Device Package item.