The Field Information Manager supports the user in exchanging a device package, even the package is a "cloud" package and has not been downloaded so far.
For exchanging the device package, i.e. from generic package to a vendor specific package, please access your device from the Topology View or Configuration View. Then open the device tile Context Menu - MORE - REPLACE DEVICE PACKAGE.
The tool will propose the best package to use. The proposed package is marked with an aim in front of the package tile. In this example, the proposed package is a "cloud" package of ABB Repository.
Be aware that the currently used package is check marked in the USED column, which is in our example the generic package.
Please accept the dialog with OK and the tool will automatically download the "cloud" package and exchange to this package. After that exchange the device is using the new package.