The sequence of Travel Time depends on the selected direction.
At the beginning of each test, the connected field device is forced into a start position which is either 0 or 100 %. From the start position, it is forced to the other end of the signal range. If configured by the direction, the field device is also forced back to the start position.
For each direction, the required time to move from one test point to another is measured. The time is measured either completely automatically in automatic execution or in between the clicks of accepting a test point in semi-automatic execution dialog.