Loop and Quality Control Performance Services improve paper mill's throughput and quality

Advanced services powered by ServicePort reduce product quality variability by 10 - 20 % and cut costs

このページをシェアする

performance-services-paper-mill

To maximize production, quality and costs management, mill managers wanted to proactively find and correct potential control issues before they could negatively affect performance

Advanced Services support leading-edge technology

An integrated pulp and paper mill in India uses leading-edge technology and processes to produce high-quality, eco-friendly products. The mill has worked closely with ABB for years, and the mill uses an ABB Quality Control System (QCS), Distributed Control System (DCS) and drives.

Product quality and throughput depend on the smooth performance of control software in both the QCS and DCS. So when mill managers learned that ABB offers services that proactively monitor QCS and automatic control, they asked ABB to demonstrate how these services could help identify potential issues and maximize productivity and quality. After seeing the service capabilities, mill managers decided to invest in ABB’s Loop Performance Service and Quality Control Performance Service, powered by ABB’s ServicePort™ Service Delivery Platform.

Challenge

  • Find and correct any automatic control problems before they negatively impact production
  • Quickly identify opportunities to improve QCS performance to maximize quality
  • Improve paper machine performance to ensure high availability

Main facts

Industry Pulp and Paper
Customer Paper mill
Country India
Solutions
 Benefits
  •  Ability to quickly diagnose problems so that productivity can remain high
  • Assurance that the mill can achieve high product quality
  • Significantly improved paper machine performance
  • Increased equipment availability

Automatic data collection and analysis

ABB Quality Control System and Loop Performance Services are facilitated through the ABB ServicePort, a secure, remote-enabled service delivery platform deployed at customer sites that allows users to view, scan and track Key Performance Indicators (KPIs) that help identify potential equipment and process problems. ServicePort automatically gathers large amounts of data, and performs initial analysis on this data to expeditiously detect trends that may indicate impending problems, so that ABB service professionals can more quickly help customers find and resolve issues that impede availability, quality and productivity.

The KPI analysis provided by these services identify, classify and prioritize issues based on severity, process area and criticality. If issues are found, customer or ABB service professionals can be alerted proactively via email or text message so that mitigating actions can be taken.

At the paper mill in India, the mill’s automatic control loops must perform as flawlessly as possible to achieve high productivity and quality. To accomplish this, mill engineers wanted to augment existing QCS and DCS services delivered by ABB with automatic data collection and analysis that would help them proactively identify emerging problems on a more consistent basis.

Loop Performance Service

ABB’s Loop Performance Service identifies and corrects automatic control loop issues to improve control performance and ensure optimum results from a control system investment. The service analyzes and identifies control loops that should be optimized so that process control can be improved and sustained.

One of the mill‘s paper machines has 220 control loops controlling the machine’s stock preparation, wet end and dry end sections. The mill‘s managers are always looking for new technologies that can help them be more competitive. So they were interested to see how the monitoring capabilities of ABB’s Loop Performance Service might detect and correct troublesome control loops.

Mill managers implemented ABB’s Loop Performance Service, and the mill uses the service to diagnose critical issues, including control output saturation, over control, slow control, signal noise and process disturbances.

After implementation, ABB demonstrated the benefits of what the Loop Performance Service identified by tuning five of the paper machine’s problematic control loops. The tuning process was tracked in detail, and mill engineers could clearly view all related data through the ServicePort Explorer, a real-time graphical user interface. After the control loops were tuned, the reduction in process variability of the loops tuned varied from 18% to 67%.

The mill’s instrumentation team has found the Loop Performance Service to be very useful in proactively diagnosing issues related to control, process and field instrumentation. Mill managers have been so impressed with the service’s benefits that they asked ABB to install a ServicePort in the pulp mill area so they can identify control loop performance issues in the chemical recovery area.

Quality Control System Performance Service

ABB’s QCS Performance Service is designed to diagnose, implement and sustain papermaking performance characteristics.

Product quality is a priority for the company, and mill managers are highly motivated to seek the most effective tools available for mitigating quality issues. They were very interested in employing the QCS Performance Service after ABB demonstrated the service’s in-depth analysis of reel data. After managers assessed how effectively the service could help them improve paper quality, they decided to implement the service on the paper machine.

Following implementation, the QCS Performance Service reel analysis indicated that moisture and conditioned weight on the paper machine had more variability than comparable industry best practices and standards. To reduce variability, ABB recommended actions that included tuning the cross-direction basis weight controller and other control loops in the wet end and stock preparation areas.

The service also showed that some sensor parameters, including the zero gap of the caliper sensor and the measurements of the basis weight sensor, were not in the expected range. Additionally, basis weight sensor noise had long-term drift. Mill personnel were able to use this information to improve sensor stability and process variability, which helped them establish the proactive system maintenance needed to avoid unplanned downtime and keep quality production high.

The periodic KPI analysis services facilitated through ABB Service Port identify, classify and prioritize issues based on severity, process area and criticality.
powered by ABB ServicePortTM

ServicePort automatically gathers large amounts of data, and performs initial analysis on this data to expeditiously find trends that may indicate impending problems, so that ABB service professionals can more quickly help customers find and mitigate issues that impede availability, quality and productivity.

Loop-performance

At the paper mill in India, the ABB Loop Performance Service tools automatically gathered and analyzed control loops based on responses to control, process and signal conditioning KPIs.

Quality Control System Performance Service

The Quality Control System Performance Service gathered and analyzed data over a three-month period, then identified, classified and prioritized issues related to measurement, control and process. The resulting Scan Report included recommendations for addressing issues to improve performance.

Better operational performance and less product waste

Using both Loop and Quality Control Performance Services, the mill has experienced fewer sheet breaks and lower grade recovery times, resulting in more saleable production.

By implementing ABB’s recommendations, mill managers expect to reduce product quality variability by 10 to 20 percent. With this improvement, they project that the mill will see gains of $75,000 to $150,000 per year through better operational performance and less product waste.

Mill managers have been so impressed with the service’s benefits that they also asked ABB to install a ServicePort in the pulp mill area so they can identify control loop performance issues in the chemical recovery area.

Learn more

  • お問い合わせ

    ご質問内容などをご入力の上、お送りください。 担当者より折り返しご連絡いたします。

    お問い合わせ
Select region / language