Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

Åsgard subsea compression system

New world record on world's first subsea gas compression system

The present state of the art in subsea power has been defined by the 310 meter-deep Åsgard field in Norwegian territorial waters. Here, the operator Statoil has just installed world’s first wet gas seabed compressor to increase pressure in the reservoir. It is estimated that it will extend the life of the Brent field by the equivalent of 306 million barrels of oil.

ABB was commissioned to provide power to the compression system, which it did by means of a cable that transmits 18 megavolt-amperes at 120 hertz over 43 kilometers. That sets a new world record for distance, voltage and frequency between a drive on a floating production facility and a seabed compressor, and points the way to what will be possible in the increasingly challenging future of subsea electrical engineering. 

Åsgard is located on the Haltenbanken of Norway in water depths of 240-310m (787-1017ft). Gas and condensate from the Midgard and Mikkel reservoirs are transported through long distance flow lines to the Åsgar A platform. 

ABB is responsible for system engineering including design, commissioning, qualification tests, measurement systems, simulations of topside drives, topside transformers and subsea transformers.

(Photo credit: Aker solutions)

Main data

Customer:  Statoil
Site:  The Halten Bank in the Norwegian Sea, Norway
Customer need:
Reliable power and control system for long distance
Scope:  Subsea transformers
Topside drives and transformers
Application: Subsea
Customer benefits
- Ensure reliable power and control for subsea gas compression system
- Ensure stable production from the Midgard and Mikkel satellite reservoirs
- Lower environmental impact
- Significantly improved safety of the operation
Commissioning year
 2015

Links and downloads