Global site

ABB's website uses cookies. By staying here you are agreeing to our use of cookies. Learn more

Complete power and control solution for $1 billion Brazilian FPSO

ABB supplies key systems for development of Peregrino field

Image ; Courtesy of Maersk Peregrino 

The Peregrino field, located 85 kilometers off the coast of Brazil, is estimated to hold about 2.3 billion barrels of heavy oil. The lead operator is the Norwegian company Statoil, with China’s Sinochem holding a 40% stake.

The field has been developed using an FSPO called the Maersk Peregrino, a vessel that was built in Singapore by marine engineer Keppel using the hull of a very large crude carrier called the Maersk Nova. The $1 billion conversion began in 2008 and was completed three years later after 15 million man-hours of work carried out by engineers of 25 nationalities, mostly based in Denmark, Norway, India, Singapore and the US.

ABB’s contribution to the project was to act as the main automation and electrical contractor. This involved the design, manufacture, installation and commissioning of the electrical, instrumentation and automation technology for the FPSO and its associated subsea equipment, as well as the telecommunication and safety systems, and the training simulators.

The power solution required a vast array of low and medium-voltage products and system. These distribute up to 72MW of power throughout the FPSO, the two wellhead platforms that supply it and the electric pumps in the production wells that are needed to lift the oil to the surface.

The peculiar challenges of producing a high viscosity reservoir include the re-injection of an immense volume of produced water combined with precise temperature management in order to keep the oil in a liquid state at all times.

The Peregrino scheme was named one of the top five offshore projects for 2011 by Offshore magazine for the “best use of innovation in production methods”.

Main data

Customer:  Statoil
Site:  Peregrino heavy crude field off the coast of Brazil
Customer need:  An integrated solution to the power and automation of a field with numerous production challenges
Scope:  Main automation and main electrical contractor for FPSO, wellhead platforms and submersible pumps
Application:  FPSO and subsea equipment
Customer benefits:

ABB was able to use its sole supplier status to integrate power and control systems and better manage the complexity of the project

Commissioning year: 2018

Links and downloads

Link
E-house