Shandong Nanshan Aluminum Co Ltd, People's Republic of China

ABB successfully commissioned coupled 3-Stand 6-High Aluminum Tandem Cold Mill

Shandong Nanshan Aluminum Co

ABB helped Shandong Nanshan Aluminum to further improve product quality and efficiency by providing a complete range of tailored automation solutions for China’s first 3-stand Tandem Cold Mill (TCM) by Shandong Nanshan Aluminum Company. 

Shandong Nanshan Aluminum Co Ltd

Shandong Nanshan Aluminum Co Ltd was established in 1993. At present, the company has many large subsidiaries and branches such as electricity, alumina, electrolytic aluminum, aluminum section, light alloy, etc., which form an industrial chain of “electricity—alumina—electrolytic aluminum—aluminum deep processing”, with strong competitive power. 

Major challenges

The mill has a capability to reduce the thickness up to 60% in the 1st stand and maximum up to 89% in one run. To fulfill the high demands, the following key technology issues have been taken into account:

  • Selection of optimal control concept with bump-less switch over according to mill mode of operation and available sensors
  • Decoupling between Roll gap, Mill drive and Flatness Control to eliminate interactions between the loops

ABB scope of supply and services

ABB has delivered the complete drive and control system for the new 3-stand 6-high aluminum tandem cold mill. ABB’s scope of work executed in project management, basic and detail engineering, In-house test, supervision for erection, commissioning and optimization.

What has been achieved?

For the main drives, ABB has used the most modern AC medium-voltage drive system “ACS6000” with unique Direct Torque Control (DTC) and ABB’s IGCT components. The drive system controls torque and speed, so that it remains fast and accurate under all operational conditions. These are important preconditions for all other technological control tasks, like thickness, flatness and tension control that results in the increased quality of the final product.

 

The new automation technology is based on the state-of-the-art ABB 800xA platform and, in addition to the peripheral units, I/O and communication modules, includes a set of high-tech controllers of the type AC 800PEC. The controller is used in all applications for rolling mills and processing lines, including technological control, drive control, plant control functions and auxiliaries. A Client / Server architecture with operator terminals was installed for process visualization and plant operation. The programming languages for the system conform to IEC 61131-3. Moreover, ABB’s migration philosophy ensures long lasting life cycle support. The advance control system applies various technological methods for controlling thickness, mass flow, tension, speed, flatness, etc.

For hardware-in-the-loop test, a mathematical process model and simulation was used in pre-commissioning of the rolling mill, which simulates the complete Tandem Cold Mill (TCM) with respect to the normal rolling mill operation from strip threading, normal operation up to tailing-out. This software enables pre-tuned control loops and secures a very smooth startup of the coil production.

The production management system implemented by ABB has different functions as following:

  • Order planning and management
  • Material tracking
  • Roll management, including data exchange to roll change robot and roll grinder
  • Quality data management
  • Product and production reports
  • Self-adapting mathematical model-based pass scheduling and set-up calculation
  • Interface to level 1, level 3 and high bay storage

In this project, self-adapting mathematical model-based pass scheduling and set-up calculation has been initiated automatically on the basis of the coil, roll and adaptation data as well as the operator trimming values and a product dependent rolling practice. Adaptive models for roll force, torque, forward slip, roll and strip temperature, thermal crown, mill stand module, roll bending and wear, are used to predict the expected process behavior in all phases of rolling and secure optimal set-up values. More than 200 set-points and control parameters are preset by the model for each coil.

 

Main data

 Customer: 

Shandong Nanshan Aluminum Co Ltd.

 Site: 

Nanshan Aluminum Plant, China

Customer need: 

  • State-of-the-art Tandem cold rolling mill complex that meets thickness and flatness quality requirements

Scope: 

  • Power system and drives, a fully integrated control system

Application: 

  • Aluminum Tandem Cold Mill
Customer benefits:
  • Achieve precise strip thickness control
  • Ensuring precise motor control, improving the dynamic performance and lowering downtime
  • Improving operational efficiency
  • Reduce maintenance costs
Commissioning year: 2012

Links and downloads

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language