Business Park cuts energy costs by 70 percent using ABB standard drives for HVAC

Two ABB standard drives for HVAC have reduced energy costs from 180 to just 50 pounds a week, giving an annual saving of over 6,000 pounds.

Share this page

To provide ventilation, the facility has an air handling unit, with a supply fan and a return fan. Each fan was directly driven by its own motor through a pulley system. The speed of each fan could be controlled by varying the ratio of the drive wheels between the motor and the fan, but this had no effect on the speed of the motor and offered no potential for saving energy.

Recent changes in activity had led to a reduced air demand. A current tenant of the center had previously been engaged in the manufacture of semiconductors, an activity that generates large amounts of heat and a subsequent demand for air circulation. As this activity had ceased, the air handling unit now had more capacity than required.

Electricity use falls by 5 percent


To save money and reduce the carbon footprint of the building, ABB Drives Alliance partner, APDS, was asked to look at the potential for using low voltage AC drives on the installation.

APDS installed two ABB standard drives for HVAC, a 22 kW drive on the supply fan and a 15 kW drive on the return fan. Running the air handling unit according to demand and taking account of the reduced occupancy, the ABB drives have reduced energy costs by 70 percent, lowering running costs from 180 pounds to just 50 pounds a week. The annual saving of over 6,000 pounds will give a payback time of 16 months. The savings were verified by the customer using the same methods employed by ABB and APDS.

business park 2
CO2 emissions have been cut by 12 tons per year.
business park

The Castlegate Business Park in Monmouthshire in Wales, UK, provides a range of accommodation for offices and light industry, including production space and storage facilities.

Facts

Customer The Castlegate Business Park
ABB channel partner  APDS
Location Monmouthshire, Wales, UK
ABB deliveries   ABB standard drives for HVAC were installed on the supply fan and the return fan, allowing the air handling unit to be run according to demand
Keys to success Energy costs are reduced by 70 percent, saving 6,000 pounds a year and CO2 emissions are cut by 12 tons per year

Find out more

Damansara City_view_small
Read the article
Damansara­ City­ upgraded ­by­ a ­Cool ­Solution
  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language