ABB's PSTX softstarter awarded for its innovative design

2015-06-22 - The new softstarting product PSTX provides more control in smaller space

    ABB proudly announces that the recently launched PSTX softstarter range has been awarded with the Product of the Year 2014/2015 medal in the category “Motors and drives” of the Polish Napкdy i sterowanie magazine. Every year the magazine dedicated to drives and control rewards a product in five categories of competition as product of the year. The publication of the winners took place during the international fair AUTOMATICON 2015 in Warsaw where ABB exhibited various products for automation, control and measurement. The jury made up of academics and the Department of Biomedical Engineering Automation AGH (Cracow Academy of Technology) awarded ABB´s PSTX softstarters with the title “Product of the Year 2014/2015” in the ninth edition of the scientific and technical magazine "Drives and Control". The main criteria to win this award was to be the most innovative product.

    image005In the category “Most innovative product” PSTX softstarters stood out due to their compact design which is one of the smallest in class while providing many included functions such as built-in bypass, torque control to prevent water hammering, backward and forward jog with slow speed as well as pump cleaning. The best in class detachable keypad can be installed on a panel door providing remote access to the PSTX softstarter and easy access to the application status by reading the display. “The PSTX team is proud to provide such an innovative product to ABB’s customers and we ensure to keep on working on high performance products. The PSTX is a compact softstarting solution so that panels can be built smaller to reduce the overall footprint,” said Carl Thorstensson, ABB´s Project leader for PSTX softstarters.

    Securing the motor reliability is one of the main benefits provided by the PSTX range. As the inrush current to start electric motors is reduced by 60 %, less stress is put on the motor thus reducing the cost of maintenance and repairs. Over ten motor protections are included to keep motors safe from overloads and network irregularities.

    Torque control, pump cleaning, jog with slow speed and many more features take motor starting to a new level. The torque control function for example is increasing application productivity by starting and stopping pumps while avoiding water hammering. The motor heating function avoids low starting temperature of the motor ensuring it to be always ready to start.

     

    http://nis.com.pl/

    http://www.automaticon.pl/english/

    http://new.abb.com/low-voltage/launches/pstx

    For help with any technical terms in this release, please go to: www.abb.com/glossary


    Speed up your process

    With advantages such as integrated muting functions and possibility to use local reset without any extra control module even the most complex safety solution is simplified. Thanks to smart solutions such as alignment help through level indication on the display and M12 contactors, installation time can be reduced. Easy diagnostics and extensive error indication further facilitate and reduce downtime.

    Improve installation efficiency

    To customize your light guard even more, Orion offers a broad set of accessories. It can simplify the installation and alignment with rotation brackets, extensive alignment help and laser pointer. Stand, deviating mirrors and different cables are other accessories which further makes Orion a flexible product for your safety solution.

    Reliable in harsh environments

    With protective tubes and lens shields, your Orion will have a long lifetime, even in harsh environments.

    Safety and protection

    By choosing a safety solution from ABB you benefit from our long experience in machine safety. We offer a complete range of safety products, which makes it easy to build safety systems. When choosing ABB you also have the advantage of the possibility to optimize your solution with only one supplier for safety, automation and robots

     
    Speed up your process

    With advantages such as integrated muting functions and possibility to use local reset without any extra control module even the most complex safety solution is simplified. Thanks to smart solutions such as alignment help through level indication on the display and M12 contactors, installation time can be reduced. Easy diagnostics and extensive error indication further facilitate and reduce downtime.

    Improve installation efficiency

    To customize your light guard even more, Orion offers a broad set of accessories. It can simplify the installation and alignment with rotation brackets, extensive alignment help and laser pointer. Stand, deviating mirrors and different cables are other accessories which further makes Orion a flexible product for your safety solution.

    Reliable in harsh environments

    With protective tubes and lens shields, your Orion will have a long lifetime, even in harsh environments.

    Safety and protection

    By choosing a safety solution from ABB you benefit from our long experience in machine safety. We offer a complete range of safety products, which makes it easy to build safety systems. When choosing ABB you also have the advantage of the possibility to optimize your solution with only one supplier for safety, automation and robots

     

Learn more about

Select region / language