Busch-Smoke alarm detector ProfessionalLINE

A safe decision

rm-rauch-abb

A fire always occurs unexpected. And very often during the night. Particularly when everyone is asleep do fires in private homes become a deadly hazard, because a persons does not smell anything while asleep. Similar to a dog. That's why it is reassuring to know that a Busch-Smoke alarm detector is keeping watch. With absolute reliability around the clock it wakes everyone in the house at the slightest indication of smoke - loudly and in time.

Optimum protection with networking


A protective network for your safety. The best smoke alarm over several floors in houses and apartments is useless if it cannot be heard. If it is too far away. To this we object: with smoke and heat detectors that are easy to network. They provide safety from the cellar to the roof. Whether wired or radio controlled: if one detector recognizes a danger, all installed devices alert the residents immediately - irrespective of where the smoke is located. This increases safety enormously, especially at night if not all rooms are being used.

A connection to external systems such as vibrating pillows for the blind or light signal devices for the deaf, but also to KNX is possible at all times via the Busch-Smoke alarm detector relay.

Also in case of radio controlled networking, each single alarm unit is directly connected with all the others. If this is not possible for structural reasons, the next detector retransmits the radio signal (repeater function). The triggering smoke or heat alarm differs from the other devices in the house by means of a flashing alarm light. It is a safe network for your protection, because thanks to the lithium batteries that are permanently installed in the radio control module and which have a service life of ten years, the full functionality is of the networked alarm units is assured even during a mains power failure.

pl-rm-rauch-01-abb

Main benefits

  • The Busch-Smoke alarm detector ProfessionalLINE is available in different versions
  • Our Busch-Smoke alarm detectors ProfessionalLINE fully conform to the highest requirements - according to standards EN 14604 and DIN 14676
  • Battery cannot be removed for other purposes; no theft possible in public buildings or social dwellings, no misuse possible as a toy in children's rooms
  • Two of them have been tested according to vfdb 14-01 and VdS 3131 and certified with the new "Q" label: an independent, vendor-neutral quality mark for high-quality smoke alarm detectors, which have been tested especially for long-term use
  • They are completely reliable

Main features

  • Battery permanently installed (sealed-in) with a service life of ten years
  • Audible alarm with 85 dBA at 3 m
  • Depending on the model: Networkable via two-wire line for up to 20 detectors
  • Test every 16 seconds, without display, suitable for bedrooms
  • VdS certification (German organisation of property assurers)
  • Smoke chamber has contamination compensation and protection against insects and it is antistatic to prevent dust from being attracted
  • Dismantling safety
  • Mute function can be activated for ten minutes;
    Slowly increasing alarm sound during function test

Highlights

Select region / language