Web story | Global | 2023-09-19 REX640 takes another step to support the transition towards digital switchgear ABB’s all-in-one protection relay for advanced power generation and distribution applications, REX640, releases new hardware for increased flexibility with more interface options.
News release 2023-06-21 ABB expands EcoSolutions portfolio with key technologies for energy transition and electrification ABB is delivering on its commitment to transparency and sustainability across its complete value chain. At ABB Electrification Smart Power, a key supplier of technologies for electrification and energy transition, 35% of global sales are now for products covered by both an independent Environmental Product Declaration (EPD) and the company’s EcoSolutionsTM information label and QR code. ABB’s
Web story 2023-05-30 Relion® REX610 expands to cover more application areas – introducing motor and arc protection Designed to provide simplified yet optimal protection and control for basic power distribution applications, REX610 takes the next step in protecting people and processes.
News release 2023-05-17 ABB Frosinone embeds sustainability throughout value chain for circuit breakers ABB Electrification Smart Power’s production hub in Frosinone, Italy demonstrates how ABB is embedding sustainability across its complete value chain – and how ABB solutions help sites achieve continuous reductions in Scope 1 and 2 emissions and energy costs. Guided by ABB AbilityTM Energy Manager insights, ABB has improved the energy efficiency of each circuit breaker it produces at Frosinone by
Web story | Global | 2023-02-20 REX640 introduces high-speed transfer to secure electrical supply for critical parts of the power system The capability of REX640 to perform automatic high-speed transfers ensures fast recovery of electrical supply for critical loads, minimizes the impact on the manufacturing process – and saves money.
Web story 2022-09-15 Relion® REX610 – now released and ready to protect any basic power distribution application Packed with innovative simplicity, REX610 is designed to simplify protection and control as the power grid evolves.
Trade press release 2021-05-18 ABB’s new all-in-one protection relay offers innovative simplicity As the power grid evolves, REX610 is designed to simplify protection and control of basic power distribution applications.
Web story 2021-03-25 REX640 introduces cost-effective switchgear HMI for optimal visibility and operational safety Capable of covering up to 20 REX640 relays, the new switchgear human-machine interface (SHMI) provides optimal visibility and reduces relay costs by up to 15 percent.
Web story 2020-11-12 Upgrade of SSC600 enables cost-effective direct communication with control center Introducing support for the remote communication protocol IEC 60870-5-104 reduces the number of components in the distribution network and the amount of engineering.
Web story 2020-10-20 Savon Voima Verkko selects ABB’s latest protection relay technology to renew substations in Eastern Finland Finnish utility provider, Savon Voima Verkko, has selected power protection solutions from ABB to upgrade its Leppävirta substation.