Steel pursues its sustainable path

Luis Pinchete, ABB's Metals Business Line Manager for Latin America, discusses steelmakers efforts towards achieving net zero emissions by 2050 as set out in the Paris Agreement on climate change.

This article was first published in Conexão Mineral Ed. No. 455, on April 22, 2024.
Steel production accounts for 7 to 9 percent of global CO2 emissions and consumes around 8 percent of the world’s energy, making it a segment that is hard to decarbonize, but one that is nevertheless determined to adopt more sustainable production practices.

The steel industry is among the signatories of the Paris Agreement and aims to be emission-neutral by 2050. This will only be achieved if the sector undergoes a profound technological transformation to mitigate emissions and become more efficient, which is already underway.

Simply put, steel is formed by mixing iron ore, sometimes scrap, and a source of carbon such as coal in furnaces that, in most parts of the world, still operate on mineral coal. In the furnace, these materials are melted into a first version of liquid steel, which receives the addition of quicklime to agglomerate and remove unwanted residues.  Only then is it cooled, rolled, and industrially transformed into its final application.

Share this page

Want to learn more about the journey towards more sustainable steelmaking?

Contact us
Luis-Pinchete

Luis Pinchete, ABB's Metals Business Line Manager for Latin America.

Conexao-Mineral-hero-image

Steelmaking is undergoing a historic transformation – and one that requires collaboration at all levels in the global steel supply chain to be successful.

In this process, there are inevitably emissions. Iron ore extraction is particularly difficult to decarbonize while coal and quicklime production also generate considerable emissions. The rolling and final transformation of steel requires a large amount of energy, most often of fossil origin. Nothing compares, however, to burning mineral coal in blast furnaces, responsible for almost the entire carbon footprint of the metal. For this reason, the sector is urgently seeking to decarbonize this stage of the steel manufacturing process.

Around the world, many steelmakers have been able to replace mineral coal with less polluting sources of carbon. Brazilian metals producer Aperam, for example, plants 100,000 hectares of forest primarily to supply charcoal for its blast furnaces. This, together with the fact that these forests also sequester and store carbon in the soil, is significantly reducing emissions ahead of adopting green hydrogen as an energy source, which Aperam plans to do when the fuel becomes more widely available.

Aperam uses charcoal produced from its own 100,000 hectares of FSC®-certified forests in Brazil as a renewable substitute for coal-based coke in steelmaking. Charcoal helps to significantly reduce CO₂ and entirely eradicate the use of extractive coal.

U.S. based Boston Metal and Swedish steelmaker SSAB are among the first in the world to use electric arc furnaces, which are fueled by electricity and have a carbon footprint up to 95 percent lower than coal-fired blast furnaces. However, the electric arc furnace is difficult to implement in many parts of the world because it depends on abundant, cheap, and necessarily clean energy (wind, solar, and green hydrogen) to make sense.

These examples show that viable technologies to reduce and mitigate emissions already exist, though the limited supply of clean energy is currently acting as a bottleneck to adoption of electric arc furnaces in the steel industry globally. Only 12 percent of the global energy matrix is wind and solar power, sources that can effectively be expanded without the environmental impact associated with hydroelectricity. The availability of green hydrogen is also growing but still far from becoming a real alternative.

The Boston Metal and SSAB examples mentioned earlier illustrate how important close collaboration with clean energy providers, willing to guarantee supply of green electricity, is to the success of pilot projects for fossil-free steel production lines. The Swedish company, for example, expects to be able to implement a fossil-free steel production line on a commercial scale by 2026, which is considered feasible.

Furthermore, these companies have found customers willing to pay a premium for their fossil-free steel, which helps finance the objectively higher production cost during this transitional phase. This is, of course, not the reality of all companies, though it does give a clear indication that the steel industry and its customers have already decided to embrace decarbonization of the metal.

SSAB-fossil-free-steel

Steelmaker SSAB, state-owned iron ore miner LKAB, and state-owned energy company Vattenfall in Sweden collaborate to make steel using green hydrogen and fossil-free electricity using the high grade iron ore from the LKAB mines instead of coking coals.

It is also necessary to highlight the decarbonization initiatives that have been taking place at the mining stage, where there is ongoing research to develop new ways of processing iron ore to facilitate its conversion into steel during primary metals production, with less energy use and CO2 emissions.

Indian company Tata Steel, for example, has developed a cost-effective process that transforms iron ore into powder, which is purer and can reduce emissions in blast furnaces by up to 10 percent. In parallel they are modernizing equipment to operate with natural gas, which is less polluting than mineral coal, while pursuing the goal of being carbon neutral by 2045.

Swedish mining company LKAB has also developed an ore enrichment method that removes part of the impurities while the raw material is still in the mine. This application was even used to produce the world's first batch of emissions-free steel in 2021, melted in electric arc furnaces operated by SSAB and ultimately acquired by Volvo Group.

Brazilian mining operator Vale has also developed a method of iron ore briquetting, which basically produces briquettes with higher iron content and allows emissions in blast furnaces to be reduced by 10 percent. There are also efforts to lower the carbon footprint of quicklime, used to aggregate slag in liquid steel.

These actions, I emphasize, already provide the steel sector with the means to produce net-zero emissions steel, but not without a lot of investment. Efforts to digitalize and automate steelmaking operations are very important here, and can even generate extra capital to finance the transition and make the numbers add up.

Strategically prioritizing efficiency improvements has proven to be especially relevant among Chinese steelmakers who, without access to significant amounts of green hydrogen and clean electricity, have sought to build and modernize plants with digital and automation solutions, optimizing operations from both financial and environmental perspectives.

This look towards digitalization has allowed several companies in Asia to identify and overcome a series of losses and inefficiencies that many plants around the world will only realize when they themselves intensify their automation processes.

The industry has come to the realization that there is no singular solution to decarbonizing operations, and that a broad approach involving the consistent application of multiple existing and emerging technologies that increase efficiency will be essential. A single piece of equipment, such as the electromagnetic stirrer, improves metallurgical performance in electric arc furnace, and can reduce energy consumption and related carbon emissions by 3 to 5 percent.

It may seem not much, but over the years, this saving represents millions of dollars in profit, which justifies investment in the equipment and allows companies to contribute to carbon footprint reductions in other manufacturing stages.

It is true that much still needs to be done for fossil-free steel to become a reality on the world market. But fortunately, transformation is taking place and it looks like there’s no going back.  That’s good news for our planet.

Learn more

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language