How best to integrate battery electric vehicles in mines

Integrating battery electric vehicles constitutes the final stage in the journey to all-electric mines and helps operators to reduce CO₂ emissions and improve efficiency. Partnering with trusted technology and equipment vendors is the key to success, write Mehrzad Ashnagaran and Nic Beutler of ABB.

slider-image_arctic
First published in the July / August 2021 issue of Global Mining Review magazine
Mehrzad Ashnagaran LinkedIn
Global Product Line Manager
Electrification and Composite Plant
Nic BeutlerLinkedIn
Global Product Manager  
Power System & Charging Solutions

The mining sector is undergoing a radical transformation driven by digitalization and electrification. Digital technologies such as the industrial internet of things, AI and data analytics now give mine operators visualization of the entire production chain, improving productivity and profitability, reducing downtime and maintenance, and informing smarter, data-driven business decisions.

In tandem, the vision of the integrated all-electric mine – one that incorporates optimal design and operations for more efficient, sustainable energy and resource consumption – is closer to becoming a reality. Central to this goal is eliminating diesel from haulage trucks, the largest source of CO₂ emissions in many open pit and underground mines, by shifting to hybrid and fully electric trucks.  

Why electrify?

Why does ABB believe that electrification is a ‘must-have’ for mining companies compared with ‘business as usual’? The industry is responsible for 4–7% of global greenhouse gas (GHG) emissions. The onus is on operators to reduce their carbon footprint to comply with increasingly strict government environmental legislation in line with the goals enshrined in the 2015 Paris Agreement.

Failure to do can result in financial penalties, the loss of competitive advantage, and reputational damage, and may also impact a company’s licence to operate. Mining operators that remain behind the curve when it comes to HSE and sustainability risk losing the backing of the board and investors, may not be permitted to work in certain jurisdictions, and could even lose their licence to operate.

In certain countries carbon taxes must already be factored into OPEX calculations as governments and industry make a compelling business case for electric mines. This shift is more advanced in underground mines, where the electrification of truck fleets has become reality and solutions such as ventilation on demand (VoD) are established innovations significantly reducing energy consumption as well as providing a safer, more amenable working environment.

The industry is part of the problem of climate change. However, by providing commodities such as copper used in wind turbines and lithium for the batteries in electric vehicles – both of which have a pivotal role to play in the global transition from fossil fuels to renewables – in a way that minimizes energy usage, resource consumption and CO₂ footprint, mining is also part of the solution. 

The three pillars of electrification

ABB’s electrical, control and instrumentation (EC&I) business has for almost half a century lead the way in mine electrification. By leveraging the technology within its portfolio and incorporating that with the latest innovations in mine engineering and design, ABB is helping to create fit-for-purpose solutions that minimize CO₂, improve safety and, ultimately, boost profitability.

ABB’s approach is built around three pillars: electrification; automation and digitalization; and being the key technical supplier (KTS) in partnership with other OEMs. What are the design requirements of electrified mines? Do they require centralized or decentralized storage systems? What are the optimum grid solutions and how can they incorporate the flexible loading of mobile equipment and integration of renewables?

The first step on this journey is to develop existing equipment and components so they are digitally enabled, and then connect them in a smart way with the flexibility to cope with supply and demand.

Open communication standards and multi-vendor integration are key to effective automation and digitalization. This means developing a single automation platform that can communicate with all the different mine assets, mobile and fixed, as opposed to a standalone architecture for each individual system. In addition, real time data acquisition and visualization allows the operator to make smart decisions and data analysis using advanced algorithms allows them to assess the state of the mine operation.

How can we embed these new technologies effectively? By putting in the third pillar, alliances of key technical suppliers and OEMs, each with their own domain expertise, to jointly develop solutions that benefit the customer, rather than one party being responsible for the whole project scope.

This is increasingly becoming the working model of choice for electrification projects, particularly when it comes to integrating a mobile fleet. At the Aitik copper mine in Sweden, for example, ABB successfully collaborated with a vehicle supplier (a third-party OEM) – which traditionally wouldn’t have worked together – to install a trolley assist line for hybrid trucks.

ABB recently signed a memorandum of understanding (MoU) with Hitachi Construction Machinery to explore opportunities to apply ABB’s electrification, automation and digital solutions to mining trucks and excavators provided by Hitachi. 

Together, the two companies hope to present a combined solution to the market that will help mining customers achieve net-zero emissions from their operations. 

ABB is also working with other OEMs to create a platform for early-stage collaboration; for example, to explore the potential of incorporating batteries into the trolley assist mix at open-pit mines.

ABB is also collaborating on electrification retrofit projects, including converting a diesel-powered Western Star 4900 XD truck with MEDATech Engineering and Tardif.  

Six ingredients for effective integration

ABB has identified six essential ingredients for the effective integration of battery electric vehicles into an existing mining operation: interoperability; mobility/flexibility; energy management; connection interface, trolley and charger technology; and favourable process and mine design. 

Interoperability

Mine fleets comprise vehicles from multiple vendors. ABB charging infrastructure is following open standards, such as CCS and OPPCharge to remain vendor-agnostic, meaning it can used across all vehicle types and OEMs. This allows the customer to make a one-off investment, and maximize the uptime, productivity and return on investment (ROI) of every piece of charging equipment. 

Mobility / flexibility

Strategically placing charging points throughout the mine means trucks remain charged for longer, optimizing their usage and overall mine productivity, and avoiding the need for additional tramming routes and vehicles. These points of charge need to be able to adapt to changes in the mine’s design throughout the lifetime of the mine.  

Energy management

Integrating battery electric vehicles into mines, the final stage of the electrification journey, means energy load requirements are much more volatile. Whilst renewables are becoming more relevant in particular for remote sites, they impose additional constraints. Smart planning of grid infrastructure and battery energy storage systems, combined with mine production forecasting, can be used to minimize load peaks and address possible volatility on the generation side. 


Connection interface

Ruggedized and mine-approved automated connection interfaces must be designed to withstand the harsh environmental conditions in many mines and high power demands of large mining trucks. This requires open mechanical and electrical standards and effective collaboration with vehicle suppliers. 

Trolley and charging infrastructure

ABB is building on existing solutions and long-lasting experience around trolley and charging infrastructure for battery electric mining vehicles. Again, these must be robust enough for the mining environment and capable of matching the high-power demands of battery electric trucks to ensure maximum vehicle uptime.  

Favourable process and mine design

Adopting new technologies will change how mines and mining assets are operated. Does the civil infrastructure and operational schedule need to be changed meet the demand of these battery electric vehicles, for example? Early-stage design thinking and planning is crucial to success.
PA_MiningKV_ppt_210615-09

Case study: Copper Mountain, Canada

ABB is working with Copper Mountain Mining to provide a complete haul truck trolley assist solution for its Copper Mountain mine near Princeton, British Columbia. The conventional open-pit operation produces approximately 45,000 metric tons of copper equivalent per year. 

ABB is responsible for all the off-truck trolley assist infrastructure – including the overhead catenary system (OCS) design and a rectifier substation providing in excess of 12MW of DC power – as well as engineering, project and construction management, equipment supply and system commissioning. 

The trolley control system can provide connectivity to the existing distributed control system (DCS) automation platform, allowing for seamless integration and monitoring of trolley operations and energy consumption.  

It is estimated that Copper Mountain will reduce emissions by 7% during the first phase of the project, and the goal is a 50% reduction in CO₂ during the next 5–7 years. Other benefits include better efficiency; each electric-drive truck will be fitted with a pantograph to receive external electric power, meaning they will run faster when connected to the trolley system, use less fuel and require less maintenance. 

ABB is collaborating directly with Copper Mountain and the truck OEM to deploy the 1 km proof-of-concept. This approach encompasses the entire ‘grid-to-wheel’ process, starting with the power distribution via the rectifier substation, design and execution of the overhead line, installation and civil work, and the creation of the surrounding infrastructure. 

In this way, if future retrofitting takes place, or an OEM supplies a new generation of hybrid trucks, ABB can use its electrification expertise to create and coordinate a complete integrated solution. 

ABB has already enjoyed success with trolley assist solutions at the aforementioned Aitik mine, for Boliden. ABB has designed, delivered and commissioned an effective electrical infrastructure to power several mine trucks. The lane is approximately 700 meters and is expected to save around 830 m3 diesel per year. 

The journey to electrification

Electrification is well underway across most of the mining chain. Electrifying the last puzzle piece by incorporating battery electric vehicles is still in its infancy and will require mining companies to adopt new technologies and working practices, and address challenges around planning, fleet management and skill sets. 

The benefits are clear, however. In addition to complying with regulation aimed at reducing CO₂ emissions and improving workplace safety, using diesel-electric trucks on trolley assist lines, for example, is proven to boost speed-on-grade for greater throughput, enable more efficient and proactive maintenance, and reduce heavy vehicle use for better fleet availability and longevity. 

Reducing emissions through electrification also makes good business sense. Electricity is becoming more cost competitive, and premiums are being offered by energy suppliers to incentivize its use; this, coupled with taxes on emissions and the removal of tax advantages from diesel, means that mining companies can no longer afford to be behind the curve when it comes to electrification. 

Partnering with a trusted technology provider with proven domain expertise such as ABB is key to incorporating battery electric vehicles in mines as part of the industry’s wider digital transformation, and drive sustainability, minimize carbon footprint, and optimize both production and profitability.
130 years panorama 2
  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language