リモートコンディションモニタリング遠隔状態監視でクリーンルームの環境を保護

clean-room_wafers_hitachi-abb-power-grids-semiconductors_web

パワートレイン用ABB Ability™ コンディションモニタリング状態監視は、スイスのリーディング・パワー半導体工場の継続的な生産に貢献しています

日立ABBパワーグリッドのレンズブルグ工場では半導体生産の維持にABB Ability™スマートセンサが活躍しております。クリーンルームはわずかなほこりや汚染によって製品の品質維持が出来ません。スマートセンサ導入により、生産中に立ち入れない機器等の遠隔監視が可能になったことで、ファン、コンプレッサー、ポンプ他生産設備計55台のモータと5台のドライブを含めたパワートレイン全体の監視ができ、従来のタイムベースからコンディションベースのメンテナンスへの移行に成功しました。メンテナンス形態の変化により、大幅なコストカットと生産性の向上が期待できます。

詳細は以下原文をご覧ください。

 

Smart sensor technology is helping avoid costly clean room closures by indicating any potential issues with powertrain equipment within air handling units (AHUs), cooling towers, and other heating, ventilation and air conditioning (HVAC) system components.

Two sealed and self-contained AHUs each feature a fan which is critical to ensuring precise temperature and humidity control inside Hitachi ABB Power Grids’ power semiconductor clean rooms in Lenzburg, Switzerland. Manufacturing thin silicon wafers in order to produce highly sensitive power semiconductor devices and modules requires a dust-free environment. Even the slightest contamination or environmental change can ruin the entire production.

Both AHUs run on partial load. If one unit fails or needs repair, the facility can ramp up the other unit to ensure continuous operation. Fitted to each of the fan motors is an ABB AbilityTM Smart Sensor to remotely track its condition.

“Most of the fans are housed in self-contained air handling units or cooling towers,” says Thomas Keusch, Facility Manager at the Hitachi ABB Power Grids semiconductor plant in Lenzburg, Switzerland.  “Direct access is not possible without shutting down the air handling unit. Being able to monitor the condition of these motors means we are better prepared to predict and schedule our maintenance needs.”

Fifty five other motors on fans, compressors and pumps, along with five variable speed drives are also enabled for remote condition monitoring. This allows the plant to remotely check the operation and health of the entire powertrain through an integrated, one-stop portal. With such data, system efficiency can be optimized, and maintenance activities planned according to actual needs rather than generic schedules. Maintenance costs can be cut, and unplanned downtime avoided.

“With integrated monitoring and analytics of all the powertrain assets, our customers can focus more on what really matters for them – manufacturing first-class power semiconductors,” says Ronald Wenger, Digital Leader, Motion business in Switzerland.

このページをシェアする

Facts

顧客

日立ABBパワーグリッド 半導体工場

場所

スイスLenzburg

産業

半導体製造業

範囲

ABB Ability™ デジタルパワートレイン
- ABB Ability™ スマートセンサ モータ向け
- ABB Ability™ スマートセンサ ポンプ向け
- ABB Ability™ 状態監視 ドライブ向け

成功へのカギ             

コンディションベースのメンテナンス

Motor fitted with Smart Sensor inside air handling unit

エアハンドリングユニット内のモータに装着されたABB Ability™ スマートセンサ

ABB motors and drives controlling the pumps

HVAC ポンプをコントロール中のABB製モータとジェネレータ

ABB motors and drives controlling the HVAC's refrigeration compressors

冷凍コンプレッサー用のABB製モータ、ドライブはABB Ability™ デジタルパワートレインと接続しています

ABBについて調べる

  • お問い合わせ

    ご質問内容などをご入力の上、お送りください。 担当者より折り返しご連絡いたします。

    お問い合わせ
Select region / language