ABB introduces TruONE to China, at ABB Customer World 2018. TruONE is an automatic transfer switch (ATS), which integrates all necessary sensors, controllers, switches and operation interfaces into one device to maximize protection, reliability, and reduce installation time by 80 percent.
When power is lost to critical equipment in hospitals, data centers or telecommunication facilities, for example, the new TruONE ATS switches automatically to a backup power source. The contact transfer is achieved in less 50 ms, which is short enough to keep loads, like lighting and motors, operational during the switch. In addition, the installation of a traditional ATS was very difficult, in that various electrical components had to be connected and assembled within a single panel or cabinet. The large number of connections and components involved made installation complicated and reduced functional flexibility and reliability.
"ABB TruONE ATS is a major innovation in engineering design and a key breakthrough in emergency power systems. It is factory assembled and fully tested, which means installation is made easy," said David Lin, Product Marketing Director, ABB China Electrification Products Division. "ABB TruONE is fully compatible with ABB Ability™ Electrical Distribution Control System (EDCS) to enable remote plant management for electrical system performance optimization and greater energy efficiency."
TruONE ATS is the first to integrate everything that critical power applications need into one seamless unit. It enables panel builders and OEMs to create high-end ATS solutions economically that can be operated manually if necessary, even under load, using an elevated handle mounted to the ATS frame, which avoids opening the panel door. This feature provides significant safety improvements. In addition dangerous line voltage no longer need be connected to the door as the detachable human-machine interface (HMI) is completely isolated from the lines providing further safety benefits to the equipment operators.
ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in power grids, electrification products, industrial automation and robotics and motion, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner in ABB Formula E, the fully electric international FIA motorsport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 147,000 employees. ABB has a full range of business activities in China, including R&D, manufacturing, sales and services, with 18,000 employees located in 142 cities, 40 local companies, and online and offline channels across over 300 cities.
For more information on ABB, please visit: http://new.abb.com/cn ABB Digital Marketing Center: https://mall.abb.com.cn Sina Weibo: @ABB Electrification Products Official WeChat Account: cnabblp