New concept in centralized protection and control for distribution substations

New concept in centralized protection and control for distribution substations

SSC600 centralizes all protection and control functionality in a single, IEC 61850-compliant device on substation level to reduce network complexity and support optimal, lifelong asset management for the digital substation.

ABB is introducing ABB AbilityTM smart substation control and protection for electrical systems SSC600 to China, at ABB Customer World 2018. SSC600 represents an innovative, centralized approach to protection and control in distribution networks. Although representing a new way of thinking, SSC600 builds on ABB’s solid and proven technological foundation manifested in the renowned Relion® protection and control family. SSC600 will be released for sale during the fourth quarter, 2018.

SSC600 has been designed to support the ABB Ability offerings of digitally enabled solutions, helping utilities and industries know more, do more and do it better than before. Combining SSC600 with other ABB Ability products and solutions offers a new way of looking at substation life cycle management. The SSC600 advanced connectivity capabilities enable seamless integration with additional services, such as remote diagnostics, asset management and upgrade services, all for great benefit of the customer.

SSC600 offers extensive application coverage with a single device for convenient station-wide visibility, minimal engineering, easy and cost-efficient process management, and advanced life cycle management for the digital substation. Combining SSC600 with merging units, which provide the measurements and physical interface between the primary equipment in the switchgear and SSC600, creates a unique, IEC 61850-compliant, centralized protection and control solution.

“SSC600 offers a fast, easy and cost-effective way to provide an existing substation with the latest technological developments within protection and control, while leaving the existing relays as backup protection,” said Alessandro Palin, Managing Director of ABB’s Distributions Solutions business. “New installations will conveniently only need bay-level merging units in addition to SSC600. Adding a second SSC600 device will create a centralized protection and control solution with full redundancy”.

The modular software allows customization at the initial ordering stage and flexible modification for the lifetime of the digital substation. SSC600 is ready to evolve alongside the grid to adapt to changing protection requirements. Continuous access to new software developments guarantees an always up-to-date substation system. The advantage of only having to modify one device instead of all bay-level protection and control devices makes upgrading the entire substation system easier than ever.

The ability to monitor and control the great variety of substation devices with one single device via a centralized human-machine interface (HMI), translates into increased situational awareness and easy access to valuable power distribution process information.

ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in power grids, electrification products, industrial automation and robotics and motion, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner in ABB Formula E, the fully electric international FIA motorsport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 147,000 employees. ABB has a full range of business activities in China, including R&D, manufacturing, sales and services, with 18,000 employees located in 142 cities, 40 local companies, and online and offline channels across over 300 cities.

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp