All-in-one protection relay for advanced applications

The fully modular, adaptable all-in-one protection and control relay REX640 makes protecting all your assets in advanced power generation and distribution applications easy throughout the relay’s life cycle.

ABB introduces a new member to its prominent Relion® protection and control family of relays for digital switchgear to China, at ABB Customer World 2018. REX640 is the outcome of a long-standing evolution and builds on ABB’s strong heritage of freely configurable multifunctional relays.

REX640 covers the full range of utility and industrial applications and is able to manage multiple applications simultaneously. This guarantees flexible, versatile and cost-efficient protection solutions. In brief, REX640 resets the standards of what is possible with a protection and control device.

The modularity and scalability of both software and hardware not only allow full customization freedom but now also unequalled flexibility in modification over the lifetime of the relay. REX640 is ready to adapt to changing protection requirements, anytime. New software and hardware developments will be continuously and easily accessible. This is asset management at its best.

“REX640 is the outcome of an evolution that will revolutionize the world of distribution protection and control,” said Alessandro Palin, managing director of ABB's Distribution Solutions business. “It fulfills the efforts of many to introduce a new solution for our customers’ needs.”

REX640 has been designed to support the increasing digitalization of substations and thereby a variety of digital switchgear solutions. With a record number of local measurement channels, supporting both conventional instrument transformers and sensors, REX640 is also able to receive multiple streams of sampled measured values via IEC 61850-9-2 LE-based process bus communication.

In addition, REX640 introduces a novel, application-driven approach to the local human-machine interface (LHMI), which allows support for entirely new applications. The intuitive LHMI features a color touch screen that visualizes power distribution process information in a unique way, with increased situational awareness and maximum usability as a result.

REX640 will be released for sale during quarter four, 2018. As a member of ABB’s Relion® protection and control family of relays, REX640 further reinforces Relion’s decade-long position as the range of relays to rely on.

ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in power grids, electrification products, industrial automation and robotics and motion, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner in ABB Formula E, the fully electric international FIA motorsport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 147,000 employees. ABB has a full range of business activities in China, including R&D, manufacturing, sales and services, with 18,000 employees located in 142 cities, 40 local companies, and online and offline channels across over 300 cities.

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp