- Latest ABB Gearless Conveyor Drive model will increase availability and energy efficiency on the existing conveyor
- ABB installation team will work at an underground station where space and transport options are limited
- Technology will support increased production on a system that already hauls 80 percent of the Malmberget mine’s iron ore
LKAB has awarded ABB a contract to install two ABB Gearless Conveyor Drives (GCDs) on the existing conveyor belt system at its Malmberget mine near Gällivare, Norrbotten County, Lapland, the most northern province in Sweden.
The existing setup already carries up to 15 million tons of iron ore every year, using a 2,800kW wound rotor induction motor (WRIM) with gearbox to drive the conveyor. It will be replaced with ABB’s latest GCD technology, two 1,600kW models with permanent magnet motors (PMM), to enable an increase in annual production while reducing energy consumption per ton.
ABB’s installation engineers and project management team face the challenge of working in a tight space at around 1,250 meters underground to remove the large equipment and replace it with the new units. Once the upgrade is complete in 2025, LKAB will be able to achieve overall energy savings of between 6 and 10 percent, which will translate to considerable OPEX savings per year.

LKAB is running a conveyor system that carries 15 million tons of iron ore every year. Image LKAB 
For personnel in the mine, the upgrade will mean reduced noise and heat in the conveyor drive area. Image LKAB 
LKAB will be able to achieve energy efficiency savings of between 6 and 10 percent with the new drives in place. Image LKAB 
An overview of LKAB's Malmberget mine, one of the largest operations of its kind in Europe. Image LKAB
ABB GCDs have a motor power of between 0.2MW and 8MW, removing the need for a gearbox and thereby lowering maintenance costs while improving overall reliability and leading to greater uptime. A unique ABB innovation, they are known to be the most energy-efficient conveyor drive solution.
“We are managing the largest iron ore mines in Europe where productivity must remain high while energy efficiency increases,” said Pär Sundqvist, Engineer and Project Owner, LKAB. “This important upgrade will improve the throughput on the conveyor and help us to meet our energy targets. ABB’s technology will also reduce both OPEX per ton and ongoing lifecycle costs.”
“The new ABB equipment will allow for an improved working environment in the mine – cleaner and safer,” said Ulf Richter, Product Manager Conveyor Solutions, ABB. “Gearless Conveyor Drives are known to be the most energy-efficient solution for conveyors, enabling reliable transportation of ore. The upgrade also means reduced noise and heat in the conveyor drive area.”
The GCD’s PMM are directly coupled to the existing conveyor’s drive pulley and can also adapted to meet the particular demands of this underground installation. The main advantages are energy savings, health and safety improvements, reduced maintenance costs and steady, solid production due to higher reliability.
ABB was awarded the project contract in the third quarter of 2023 and the installation will take place during scheduled maintenance stops with the final commissioning due in August 2025.
ABB’s Process Automation business automates, electrifies and digitalizes industrial operations that address a wide range of essential needs – from supplying energy, water and materials, to producing goods and transporting them to market. With its ~20,000 employees, leading technology and service expertise, ABB Process Automation helps customers in process, hybrid and maritime industries improve performance and safety of operations, enabling a more sustainable and resource-efficient future. go.abb/processautomation
ABB is a technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. The company’s solutions connect engineering know-how and software to optimize how things are manufactured, moved, powered and operated. Building on more than 140 years of excellence, ABB’s ~105,000 employees are committed to driving innovations that accelerate industrial transformation.www.abb.com