The drive for decarbonization is causing industrial businesses across North America to electrify their operations by switching from diesel-fuelled pumps to systems powered by electric motors. This is especially true in the chemical and energy industries where there is a major trend to deploy heavy-duty horizontal electric pumps. To meet this demand ABB has developed the new ECP5000 series Severe Duty motors to provide exceptional performance and maximum uptime in harsh industrial processing applications.
Until quite recently, operators in North America regarded medium voltage (MV) technology, typically at 4 kilovolt (kV) or above, as essential for their high-power motors. This started to change with the growing adoption of variable frequency drives (VFDs) that offer very significant energy savings. Using a high-power LV motor together with an LV drive provides a more cost-effective solution than MV equipment.
The capability of the ECP5000 series Severe Duty motor to deliver up to 1000 Hp (745 kilowatt) has been achieved by a process of evolution rather than revolution, as Robert Boyce, ABB Local Division Manager, IEC LV Motors – US, explains: “High power, low voltage motors are well established in IEC markets. So, our challenge was to put this wealth of knowledge into a format with mounting dimensions and shaft height to match the existing installed base. To do this we stripped the motor design down to its individual elements and optimized each one. We then used this as a set of building blocks to create our ideal, flexible design.”
Robert continues: “The key success of the ECP5000 motor is that even with the lowered shaft height we have been able to minimize vibration to ensure a long and reliable service life in the most demanding conditions. In essence, we have delivered the virtues of IEC motor design in a NEMA-dimensioned package to meet customer needs.”

Auxiliary drive end cooling fan for 2pole ratings 
ECP5000 Severe Duty motor with ABB Smart Sensor 
ECP5000 series Severe Duty motor exploded view
Attention to energy efficient design enables the ECP5000 motor to meet IE4 levels in direct online installations. This is equivalent to NEMA Super Premium Efficiency. When used with a VFD, the motor is capable of achieving IE5 according to IEC TS 60034-30-2, the highest level currently recognized.
Other advantages of the ECP5000 motor are its robust cast iron IP66 enclosure combined with a large, left hand side conduit box that can be rotated in 90-degree increments or converted to right hand side or top mounting for ease of connection.
ABB Motion keeps the world turning – while saving energy every day. We innovate and push the boundaries of technology to enable the low-carbon future for customers, industries and societies. With our digitally enabled drives, motors and services our customers and partners achieve better performance, safety and reliability. We offer a combination of domain expertise and technology to deliver the optimum drive and motor solution for a wide range of applications in all industrial segments. Through our global presence we are always close to serve our customers. Building on over 140 years of cumulative experience in electric powertrains, we learn and improve every day. go.abb/motion
ABB is a technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. The company’s solutions connect engineering know-how and software to optimize how things are manufactured, moved, powered, and operated. Building on more than 140 years of excellence, ABB’s ~105,000 employees are committed to driving innovations that accelerate industrial transformation. www.abb.com