- New range AK600 of wall-mounted consumer units launched
- Highly flexible and easy installations as with the proven UK600 flush-mounted version
- Reduced stockkeeping thanks to common doors and accessories
The popular UK600 flush-mounted consumer electrical unit now has a new accompanying wall-mounted unit, the AK600. The AK600 wall-mounted consumer unit is designed primarily for residential and small commercial applications and can be used in renovations, upgrades, and new construction. It follows the unique flexibility and ease of installation of the UK600 that has set standards in electrical installation. Created in response to customer demand, the AK600 wall-mounted consumer unit is available now. Installers can now optimally cover all conceivable requirements with the UK600 and AK600.

The AK600 offers the same features that have made the UK600 popular with installers. Outstanding features include an up to 130 percent larger connection space and integrated fastening options for cables using cable ties. More space at the top and bottom facilitate cable entry. For easy installation of cable ducts, there are discreet, easy-to-break-out wiring knockouts in various sizes at the top, bottom and sides for installation ducts and tubes.
The new AK600 is available in five sizes, with one to five rows, and with different door variants. The same doors can be used for both the AK600 and UK600, with a door frame to be added to the UK600. The AK600 is available as a consumer unit and media enclosure and can be connected horizontally or vertically.
One of the most important features of the new consumer unit is its very high flexibility. This is ensured by thought-through details such as the wire holders and the terminals that can be mounted at the top, bottom, or side. The universal patch panel for EDAT and keystone modules for data cables is also available for the new consumer unit. AK600 and UK600 share the same accessories, simplifying stock keeping. The uniform interior design and the same accessories, together with ABB's extensive product portfolio, cover all the needs of professional electrical installation.
ABB is a technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. The company’s solutions connect engineering know-how and software to optimize how things are manufactured, moved, powered and operated. Building on more than 130 years of excellence, ABB’s ~105,000 employees are committed to driving innovations that accelerate industrial transformation. www.abb.com
Electrifying the world in a safe, smart and sustainable way, ABB Electrification is a global technology leader in electrical distribution and management from source to socket. As the world’s demand for electricity grows, our 50,000+ employees across 100 countries collaborate with customers and partners to transform how people connect, live and work. We develop innovative products, solutions and digital technologies that enable energy efficiency and a low carbon society across all sectors. By applying global scale with local expertise, we shape and support global trends, deliver excellence for customers and power a sustainable future for society. go.abb/electrification