Personalised confectionery manufacturer Boomf increases product quality and throughputwith the IRB 1200
An ABB IRB 1200 robot has been instrumental in the growth of newly formed start-up Boomf, aspecialist manufacturer of marshmallow-based novelty products. Part of an automated cutting cell, therobot has helped to significantly reduce both production delays and product wastage that wereinherent in the company’s previously manual-based production process.
Started in 2013 by founders James Middleton and Andy Bell, Boomf enables its customers to printtheir choice of photos, graphics and messages on to marshmallows which they can then have sent toa chosen recipient as a quirky alternative to flowers, chocolates or greeting cards.
The idea proved so popular that within a year the company’s manual production line at its factory in Reading began to struggle to keep up with orders. Much of the delay was happening at the cutting stage. The high standards set by the company meant that each product needed to be carefully cut,causing a bottleneck in the production flow. Difficulties in achieving a consistently high quality cut alsomeant that a lot of product was being wasted.
With the company specialising in such a niche product, the founders feared that solving this problemwith automation would require custom-built equipment and machinery. In the words of James Middleton, “There was no marshmallow printing shop around the corner.”
Unique solution
James used his physical manufacturing background to begin researching solutions online. Looking at various cutting machines for the food industry on YouTube, he found a video of a robot cutting application which used an ABB six axis robot and an ultrasonic blade to cut cakes. The automated system was integrated by Newtech, an ABB Robotics UK Authorised Value Provider.
Located in Sharnbrook, North Bedfordshire, Newtech specialises in automation for the food industry and was the first company in the world to create a commercial robotic cutting solution combining a robot arm with an ultrasonic blade.
“As soon as I saw the video, I immediately realised it was the solution we needed. We got on the phone, contacted Newtech and then we went up to trial some solutions,” recalls James.
Trial and error
Like any robot installation, trials are required to ensure the best results. The inherently sticky nature of marshmallow initially proved a challenge for Newtech’s machines, which were set up to cut more solid substances such as cakes and cheese. Newtech overcame this challenge by applying a mechanically PTFE coated blade to the ABB IRB 1200. The blade passes through an oil reservoir before the cut is made in order to ensure a suitable surface for cutting. Once the marshmallow is portioned, the blade passes through a cleaning tank before repeating the process.
A clean-cut design is of the utmost importance to Boomf. James Middleton explained, “We make sure we have a precise square, not just something that’s almost a square, and we have very sharp angles and edges so that we have a good printing substrate.”
By introducing the robotic solution, Boomf has achieved major savings in both production time and wastage. When the process was performed manually, Boomf employed ten people to cut the trays of marshmallow into 40mm by 40mm squares. After every five or six cuts, the blade would need to be cleaned. In total this took five minutes.
Due to miscuts, there was also a lot of wasted product. Now that the process has been automated, the procedure takes just 17 seconds. Newtech also integrated intelligent vision software into the robot cell to ensure that Boomf would get the perfect cut each time. According to James Middleton, “There’s next to no wastage now and that’s been a real benefit to the figures.”
Jaz Gill, Sales Manager at Newtech, explained how the AVP uses vision technology in this and many other processes to accurately cut and track products as they arrive in the robot cell. “The vision technology scans images and then uses 2D vision from the top of the cell to recognise the product.The data is then sent into the robot to follow it – be it a tart, cheesecake or a sandwich. The camera ignores any other elements to achieve a perfect and accurate cut.”
Response to market
In addition to improved product quality, the robot solution has raised productivity levels significantly. Now Boomf has the flexibility to respond to changes in demand. The confectionery company receivesa large increase in orders during holiday periods such as Christmas and Valentine’s Day and needsthe resources in place to cope with fluctuations. Improving the process has also enabled Boomf to focus on other areas of the business such as expanding delivery to more countries and looking at howother processes could be automated.
Says Jaz: “We develop a partnership with our customers and look at where we can add value acrossthe whole of their production line. In Boomf’s case, we can cut the product perfectly, but they still have a challenge in manually putting the product into boxes.” Over the coming months, Newtech will begin trialling various potential solutions using another ABB robot.
Further, using an IRB 1200 within a machine cell allowed Boomf to improve the health and safety atthe site. James Middleton was a victim of the manual process before the automated system was installed. He severed a nerve in the end of his finger whilst cutting a batch with a knife. Removing the human interaction from the cutting process removes the risk of such accidents and the employees can apply their skills to other areas of the business such as operating the robot.
Overall, Newtech’s automated solution has been a real success for the company. Ease of use is ensured through the use of an HMI which enables staff to operate the cell following simple training.
Enhanced expansion
In terms of finances, Boomf was well aware that as a start up there would be a lot of cost. However, through investing in a robot the company has already experienced the benefits, and in only its second year of business has grown at an astounding rate of 600%. James Middleton added, “It’s the benefits of having the robot that’s allowed us to grow that much in one year.”
Jaz Gill firmly believes that robotics and automation in general is completely underutilised within the food and beverage industry. “It’s a whole culture change that we need to bring to our customers and their partners, for people to understand that the use of robotics, the use of automation, the intelligence, is not only far more economic than it’ ever been and yields a faster payback, it’s incredibly easy to use.”
When asked about what he would say to UK manufacturers who were thinking of investing in robotic automation, entrepreneur James Middleton was encouraging. “I’d say go for it. The success that we’ve had with our robot speaks for itself. Any investment in robotics is a great decision for any company that wants to insure their future in an increasingly digital market.”