- Collaboration with Global Peace Foundation Malaysia to benefit approximately 200 Orang Asli in Kuala Rompin, Pahang
- Contribution to fund solar-powered systems to light up homes, street lights and community spaces
In a world where technological advancements are rapidly transforming urban landscapes, it is easy to overlook the fact that many communities still live without basic amenities such as electricity. Around 270 kilometers from Kuala Lumpur, there are communities that remain in darkness once the sun sets.
According to reports, in 2024, Malaysia is home to 209,575 Orang Asli from 18 sub-ethnic groups. Most reside in Perak and Pahang, with nearly 50 percent living in poverty and 19 percent in extreme poverty.
In districts like Pekan and Rompin, the poorest among them, Orang Asli communities face critical challenges including limited access to clean water, electricity, education, and essential infrastructure. Many of these villages are located within oil palm plantations or the outskirts of towns. Deforestation has further disrupted their traditional ways of life, compromising their ability to self-sustain.
Recognizing this dire need, ABB Malaysia’s Electrification business announced its contribution to the Global Peace Foundation to help bring sustainable energy to two Orang Asli villages in Rompin, Pahang.
In Kampung Jong and Kampung Bukit Serok Lama, homes and community spaces lack access to electricity. To light their surroundings after dark, villagers often resort to burning dried palm fruits in bonfires which emit smoke that causes throat and eye irritation, especially among children. These fires also pose serious safety risks, as they can unexpectedly flare up or even explode causing injury. In the absence of street lighting, communities are also more vulnerable to wildlife encroachment.
To power basic appliances, some families rely on expensive and unsustainable energy sources such as petrol-fueled generators and disposable batteries. Heavy-duty 6V batteries are commonly used to charge phones, while generators provide limited electricity for fans and lights across a few homes. One villager, Pak Asah, spends roughly RM144 monthly on batteries, amounting to 30–40% of his income.
These practices not only strain household budgets but also cause harm to the environment. Improper disposal of batteries contributes to soil, water, and air pollution. As they corrode, toxic chemicals seep into the ground and contaminate water sources. These emissions affect respiratory health and contribute to broader climate impact.
Transforming lives
Through its partnership with Global Peace Foundation Malaysia, ABB Malaysia is supporting the installation of solar-powered systems in Kampung Jong and Kampung Bukit Serok Lama. These systems will light up homes, compounds, and communal spaces - creating safer, healthier, and more connected communities.
With the introduction of solar-powered lighting, villagers are empowered to improve their livelihoods as their productivity will no longer be constrained by daylight hours. Additionally, their safety is significantly improved, allowing families to gather after dark and enabling children to study even after sunset. This simple yet profound change opens up new possibilities for these communities, breaking the cycle of poverty and fostering hope and opportunity.
“This contribution exemplifies our commitment to social progress. By bringing light to those who need it most, ABB Malaysia is not only illuminating homes but also igniting dreams and aspirations. This donation is a testament to the power of collaboration and the positive change that can be achieved when organizations unite for a shared purpose,” said Clemens Stahl, Vice President, Smart Power and Smart Building, ABB Malaysia Sdn Bhd.
“We are deeply grateful to ABB Malaysia for supporting our mission,” said Dr. Teh Su Thye, CEO of Global Peace Foundation Malaysia. “At Global Peace Foundation Malaysia, we believe that we are all part of a larger fabric of humanity. This project symbolizes our commitment to building resilient, self-sufficient communities that can thrive.”
The project to illuminate Kampung Jong and Kampung Bukit Serok Lama will span over a period of around eight months. “The prospect of how this contribution will change lives underpins our sustainability agenda, which is to create a more prosperous and sustainable future for the communities in which we operate,” Clemens concluded.