ABB expands drive portfolio with 315 and 355 kW wall-mounted drives

ABB expands drive portfolio with 315 and 355 kW wall-mounted drives

• New frame introduces 315 kW and 355 kW ratings for ACS580-01, ACQ580-01 and ACH580-01

• Among the most compact wall-mounted drives in their power class, reducing footprint and integration costs

• Optimized for cooling, refrigeration, water and general industrial applications

ABB has expanded its all-compatible drive portfolio with the introduction of a new wall-mounted frame, extending the ACS580-01, ACQ580-01 and ACH580-01 drive ranges with new 315 kW and 355 kW power ratings. The new frame delivers up to 355 kW in a compact wall-mounted format, positioning ABB among the most compact solutions in this power class.

The new frame responds to increasing demand for higher output power combined with limited installation space. Its compact design helps reduce cabinet size, panel footprint and system complexity, lowering integration costs across a wide range of applications, including cooling and refrigeration, water and wastewater, heat pump systems, and general industrial processes.

The wall-mounted drives can be skid-mounted directly to the application or installed within cabinets, including under-unit horizontal mounting. This flexibility enables efficient integration into machine and system structures, supporting compact layouts and modular designs.

All ACS580-01, ACQ580-01 and ACH580-01 variants are available in IP21 and IP55 enclosures, making them suitable for both cabinet installation and more demanding environments. The drives are engineered for harsh operating conditions, supporting ambient temperatures of up to 55 °C (40 °C without derating) and meeting C3 (IP21) and C4 (IP55) environmental classifications for long-term reliability.

ACS580-01, ACQ580-01 and ACH580-01 wall-mounted drives, 355 kW, IP21 and IP55
ACS580-01, ACQ580-01 and ACH580-01 wall-mounted drives, 355 kW, IP21 and IP55
center

Installation, commissioning, and servicing are simplified through an optimized wiring terminal section and a patented tilting cabling box, providing fast access to internal components and improving accessibility during installation and maintenance. Offline configuration capabilities allow parameter setup and commissioning without requiring the physical drive, helping reduce overall commissioning time.

315 and 355 kW wall-mounted drives with a new, innovative wiring section
315 and 355 kW wall-mounted drives with a new, innovative wiring section
center

Application-specific functionality is supported across the drive families. For cooling and refrigeration applications, this includes dedicated compressor functionality with support for standard refrigerant tables and Antoine coefficients for custom refrigerants, enabling straightforward integration and redundancy in both new and existing systems. A2L and A3 refrigeration conformity documentation is included to support compliance with modern refrigerants where applicable.

To support sustainability objectives, Environmental Product Declarations (EPDs) are available, helping manufacturers and system integrators assess environmental impact and advance lifecycle sustainability goals.

“The demand for higher-output systems continues to grow, while available installation space is becoming increasingly limited,” said Andy Organ, Global Product Manager – HVACR drives at ABB. “By extending the ACS580, ACQ580 and ACH580 families up to 355 kW in a wall-mounted design, we help our customers build more compact, cost-effective and reliable solutions across multiple industries.”

With the introduction of the new 315 and 355 kW wall-mounted frame, ABB further strengthens its all-compatible drive platform, providing greater flexibility, higher power density and application-optimized functionality for a broad range of industrial and infrastructure applications.

The drive mounted on the compressor skid.
The drive mounted on the compressor skid.
center

ABB is a global technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. By connecting its engineering and digitalization expertise, ABB helps industries run at high performance, while becoming more efficient, productive and sustainable so they outperform. At ABB, we call this ‘Engineered to Outrun’. The company has over 140 years of history and around 110,000 employees worldwide. ABB’s shares are listed on the SIX Swiss Exchange (ABBN) and Nasdaq Stockholm (ABB). www.abb.com

ABB Motion, a global leader in motors and drives, is at the core of accelerating a more productive and sustainable future. We innovate and push the boundaries of technology to contribute to energy efficient, decarbonizing and circular solutions for customers, industries and societies. With our digitally enabled drives, motors and services we support our customers and partners to achieve better performance, safety and reliability. To help the world’s industries outrun – leaner and cleaner, we deliver motor-driven solutions for a wide range of applications in all industrial segments. Building on over 140 years of domain expertise in electric powertrains, our more than 23,000 employees across 100 countries learn and improve every day. go.abb/motion

For more information, please contact:   

Media Relations Email: media-motion@ch.abb.com

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp