ABB Ultra-Low Harmonic (ULH) Drive

ABB Ultra-Low Harmonic (ULH) Drive

Power Quality as Leverage in Malaysia's New Carbon Sensitive Landscape

Power quality is not just a technical matter — it is strategic lever to increase margins and reduce carbon risks. Particularly pertinent with the introduction of Malaysia’s carbon taxes and EU’s CBAM in 2026.

Industries should consider investing in the ABB Ultra‑Low Harmonic (ULH) drives that cut downtime and extend asset lifecycle. They have Total Harmonic Distortion of Current (THDi) that is typically less than 3% at full load, without the need for external filters. This keeps electrical networks clean while protecting transformers, switchgears, and motors, and minimise unplanned downtime.

"Harmonics are electrical disturbances created by non‑linear loads such as conventional 6‑pulse drives. By addressing harmonics directly at the source, ABB’s ULH drives prevent overheating, unexpected shutdowns, and equipment oversizing — cutting energy losses while boosting efficiency," said R Narayanan, Local Division Manager, Motion, ABB Malaysia Sdn Bhd.

The payoff is undeniable for operators navigating carbon‑linked costs and CBAM‑ready exports – translating into measurable efficiency gains, improved power stability, and enhanced competitiveness

In a nutshell, ABB ULH drives turn power quality into an advantage in Malaysia’s new carbon‑sensitive landscape.

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp