- ABB Robotics launches simplified version of its PickMaster software for packaging OEMs and system integrators to speed up and simplify the development of robotic picking solutions
- Easy-to-use essential features reduce engineering by 30% and commissioning and deployment time by 25% while delivering proven ABB high-speed, vision-guided picking performance
- A simple, scalable way to bring reliable vision‑guided picking to market – fast to deploy and ready to perform
ABB Robotics today launched PickMaster® Lite, a streamlined version of its PickMaster software suite designed to help packaging OEMs and system integrators deploy high-speed, vision-guided robotic picking applications more quickly and with less complexity. Offering essential functionality for common picking tasks, PickMaster Lite reduces engineering effort and simplifies system setup, enabling faster commissioning and lower total cost of ownership.
“Manufacturers are increasingly looking for automation that can be deployed quickly and reliably to keep pace with changing demand,” said Craig McDonnell, Business Line Managing Director Industries at ABB Robotics. “With more than 74 percent of manufacturers facing ongoing labour shortages1, and nearly 80 percent of consumers expecting more personalised products2, the pressure to increase production flexibility is growing. PickMaster Lite enables machine builders to bring robotic picking systems online faster, while maintaining the performance and flexibility required for high-speed applications.”
A streamlined version of ABB Robotics’ proven PickMaster technology, PickMaster Lite delivers accurate vision-guided picking, conveyor tracking, and motion control through an intuitive, task-based interface. Pre-configured templates and guided workflows remove the need for specialist programming expertise, reducing engineering effort by 30 percent and commissioning time by 25 percent in comparison to conventional pick-and-place software or PLC based.
PickMaster Lite can also be integrated with ABB Robotics’ RobotStudio® platform, enabling users to create digital twins, simulate layouts, and optimise robot paths prior to installation. Together, these features provide a simpler, lighter, and lower-risk development path for compact, scalable, high-speed vision-guided picking cells and machines.
PickMaster Lite is designed to integrate easily into existing machine control architectures, enabling seamless communication with PLC and HMI systems via the OmniCore™ controller. This allows machine builders and system integrators to manage key functions such as recipe selection, start, stop and pause directly through their preferred control systems, allowing OEMs and system integrators to maintain existing machine designs while reducing development risk.
PickMaster Lite is ideally suited for cost-sensitive, high-volume standard picking and packing cell applications where simplicity, speed and reliability are critical, such as consumer goods, food and beverage, pharmaceuticals, electronics and e-commerce.
As part of the PickMaster family, PickMaster Lite provides a scalable pathway from simple set-ups to more advanced solutions using PickMaster and PickMaster Twin, enabling users to expand functionality as their production needs evolve. For more advanced needs, PickMaster delivers enhanced functionality, greater customization and higher performance for complex picking tasks, while PickMaster Twin extends capabilities further through digital twin technology, enabling simulation, testing and real-time optimization of live picking lines.
For more information, visit PickMaster Lite website.
References:
[1]. Source: World Manufacturing Foundation - ‘2024 World Manufacturing Report - new perspectives for the future of manufacturing: outlook 2030’
[2]. Source: Deloitte - ‘Unlocking customer growth: Driving high value actions through personalization and retail media’
ABB Robotics as one of the world’s leading robotics companies, is the only company with a comprehensive and integrated AI-powered portfolio covering robots, cobots and Autonomous Mobile Robots (AMRs), designed and orchestrated by our value-creating software. We help companies of all sizes and sectors - from automotive to electronics and logistics – to outperform by becoming more resilient, flexible and efficient. ABB Robotics is at the forefront of developing and commercializing a new generation of Autonomous Versatile Robotics (AVR), leading a global innovation ecosystem of partners in advancing efficient hardware and intelligent software with industrial performance. The business employs approximately 7,000 people. go.abb/robotics