ABB introduces new solution to automate quay crane waterside operations and improve container terminal efficiency

ABB introduces new solution to automate quay crane waterside operations and improve container terminal efficiency

  • ABB’s Waterside Automation solution enables transition toward autonomous ship-to-shore crane operations, reducing reliance on continuous manual control and addressing a key bottleneck at container terminals
  • Combines sensor data, AI and integrated operational functions to automate operation over the vessel and ensure consistent execution of the full handling cycle
  • Enables operators to be decoupled from individual cranes, allowing terminals to improve workforce flexibility while introducing quay crane pooling

ABB introduces Waterside Automation solution which enables quay cranes to perform a larger share of container handling operations automatically. By automating operations over the vessel and reducing the need for continuous manual control, the solution addresses a key bottleneck in container terminal efficiency and enables a gradual transition toward autonomous quay crane operations.

Today, facing ever-increasing pressure on schedule reliability, many container terminals have already automated much of their yard operations. Quay cranes, however, still rely heavily on manual control, which can limit overall productivity. Drawing on ABB’s expertise in system integration and artificial intelligence, ABB’s Waterside Automation solution increases the level of automation in quay crane operations over the vessel, making the process more consistent and reducing interruptions caused by manual interventions.

A key feature is that the solution enables decoupling of the operator from individual quay cranes. Instead of directly controlling challenging activities like picking up and setting down containers over the vessel, operators will be able to supervise the process and manage multiple cranes from an office environment, allowing terminals to introduce quay crane pooling. This also helps improve workforce flexibility.

ABB’s Waterside Automation solution integrates vision- and movement-based sensor technologies with data analytics and AI to control container position, crane movements, and the vessel environment in real time. Based on this data, the system can automatically execute lifting and positioning tasks, while ensuring safe and consistent crane operations under changing conditions including vessel movements both alongside and across the quay, as well as the impact of weather. It also connects with other handling processes and operator interfaces, helping to coordinate container flows and increase operational efficiency across the terminal.

While similar sensor- and AI-based technologies have been developed and deployed in urban environments, such as semi-autonomous vehicles in public transport systems, ABB has adapted and validated these capabilities specifically for container terminal operations. Crucially, the solution integrates exception handling, stowage confirmation, optical character recognition (OCR), and digitalized work instructions into a coordinated system. This reduces the need for manual verification between steps and supports consistent execution across the full crane cycle.

“ABB, as a system integrator, is in a unique position to deliver this solution and facilitate a stepwise transition towards autonomous quay crane operations,” said Thomas Kumm, Global Technology Manager, Ports, ABB’s Marine & Ports division. “We design and develop our systems to evolve in line with terminal operations and technological development and continue to add new functions as requirements change.”

ABB is a global technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. By connecting its engineering and digitalization expertise, ABB helps industries run at high performance, while becoming more efficient, productive and sustainable so they outperform. At ABB, we call this ‘Engineered to Outrun’. The company has over 140 years of history and around 110,000 employees worldwide. ABB’s shares are listed on the SIX Swiss Exchange (ABBN) and Nasdaq Stockholm (ABB). www.abb.com

ABB’s Automation business automates, electrifies and digitalizes industrial operations that address a wide range of essential needs – from supplying energy, water and materials, to producing goods and transporting them to market. With its ~26,000 employees, leading technology and service expertise, Automation helps process, hybrid and maritime industries outrun – leaner and cleaner. go.abb/automation

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp