ABB expands proven SD200 841 motor line to offer more power for severe duty processes

ABB expands proven SD200 841 motor line to offer more power for severe duty processes

Expanded horsepower range - SD200 841 now rated to 500 Hp

Standardized terminal blocks - Factory-installed terminal blocks on all FS500 motors for consistent, reliable installation

Full IEEE 841 compliance - Severe-duty performance for chemical, petrochemical, mining and pulp and paper environments

ABB has expanded its SD200 841 severe-duty motor line to 500 horsepower. New, larger frame sizes provide more power for demanding applications while maintaining full IEE 841-2021 compliance. Designed for harsh operating environments, the motors provide the rugged performance, reliability and long service life required in severe-duty service. 

ABB’s SD200 841 line is engineered to meet or exceed IEEE 841-2021 requirements for efficiency, performance, construction, variable-speed operation and long service life. With the addition of larger 5000 series NEMA frame sizes 5009 through 5013, the platform now spans 75 to 500 Hp. The expanded range extends beyond the previous 449T frame size, providing greater horsepower coverage for large industrial applications operating in harsh environments. 

center

Built for demanding environments 

ABB’s SD200 841 delivers IP56 protection for operation in wet and contaminated environments. Class H insulation provides increased thermal capacity to support longer motor life in high-temperature applications.   Bearing isolators on both drive and non-drive ends help prevent contamination and reduce unplanned maintenance. Motors operate at low vibration levels of 0.06 IPS, supporting smooth, efficient performance in high-torque applications.  Each motor ships with an IEEE 841 test report and is backed by a five-year warranty.  Safety certifications include UR component recognition and CSA listings for Class I Division 2 and Class II Division 2 hazardous locations.  An oversized conduit box and field-modifiable design simplify installation, connection and maintenance. The new 5000 frame size motors also feature factory-installed terminal blocks as standard, replacing traditional flying leads. This enhancement improves connection reliability, simplifies installation and provides easier access for maintenance. 

Applications 

The ABB SD200 841 FS500 is purpose-built for petroleum and chemical plants, pulp and paper mills, mining and aggregates operations, cement production facilities and industrial process pumping and conveying applications where reliable high-horsepower performance is critical.  The expanded lineup allows facilities to standardize on a single IEEE 841 motor platform across a broader range of equipment, helping improve reliability, reduce maintenance and extend service life as horsepower requirements increase.  Learn more about ABB's SD200 841 severe-duty motors at abb.com.

center

ABB Motion, a global leader in motors and drives, is at the core of accelerating a more productive and sustainable future. We innovate and push the boundaries of technology to contribute to energy efficient, decarbonizing and circular solutions for customers, industries and societies. With our digitally enabled drives, motors and services we support our customers and partners to achieve better performance, safety and reliability. To help the world’s industries outrun - leaner and cleaner, we deliver motor-driven solutions for a wide range of applications in all industrial segments. Building on more than 140 years of domain expertise in electric powertrains, our more than 23,000 employees across 100 countries learn and improve every day. go.abb/motion 

ABB is a global technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. By connecting its engineering and digitalization expertise, ABB helps industries run at high performance, while becoming more efficient, productive and sustainable so they outperform. At ABB, we call this “Engineered to Outrun.” The company has more than 140 years of history and around 110,000 employees worldwide. ABB’s shares are listed on the SIX Swiss Exchange (ABBN) and Nasdaq Stockholm (ABB). www.abb.com 

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp