By Adam Mease, Business Line Leader, Energy Distribution NEMA, Smart Buildings
This is the first in a series exploring the decisions that matter most in residential electrical design right now. From load management and circuit protection to modular installation and the labor pressures reshaping how homes are built.
Residential electrification is entering a new phase, one defined by scale, speed, and rising expectations. Heat pumps. EV chargers. Battery storage. Solar panels. What once felt like optional upgrades are now landing on active job sites across North America, driven by homeowner demand, policy pressure, and code changes moving faster than many in the industry anticipated.
The homes being delivered today look nothing like the ones the electrical industry was built to support. Builders, electricians, and developers are navigating the same fundamental challenge: the electrical infrastructure running most homes simply wasn't designed for what's being asked of it.
Here are four reasons why the shift is already underway.
1. Codes are being designed for an electric-first future
The NEC 2023 cycle is now effective in 26 states1. New York's All-Electric Buildings Act is phasing in. Future codes like the 2024 IECC are designing around electrification from the ground up. This isn't just about compliance, it's a signal that homes permitted in the future will require more capacity, greater flexibility, and smarter control than any previous generation.
2. Electrical demand inside homes is accelerating
Even before the current wave of electrification, household electricity consumption rose 40 percent over the last 40+ years.2 With widespread adoption of electric heating, water heating, and transportation now underway, demand is expected to grow another 10-15 percent in the next decade alone.3
Four million heat pump units shipped last year, surpassing gas for the first time. Electric water heaters are rising as gas declines. Yet 60–70 percent of US homes still have panels rated below 200 amps4, panels that were never designed for these loads. The gap between what homes were built to handle and what they're now expected to support is widening every year. Builders who aren't designing for this are building homes that will feel outdated long before they should.
3. Safety requirements are expanding as loads get more complex
Modern codes continue to increase requirements for Arc Fault Circuit Interrupters (AFCI), Ground Fault Circuit Interrupters (GFCI), and dual-function protection. Breakers now need to safeguard more circuits simultaneously and respond with greater precision – minimizing unnecessary interruptions while safely handling larger, fluctuating loads. This means smarter, more sophisticated products that provide elite technology while prioritizing safety in the home.
4. Labor shortage is forcing a rethink of how systems are designed and installed
The skilled labor shortage is already here with 77% of US construction firms report difficulty hiring electricians5. That's reshaping how homes are built. On job sites across the country, simplicity has become as valuable as capacity. Every additional wiring complexity adds time, coordination pressure, and risk of error or failed inspection. This is driving real demand for modular panel designs and simplified wiring layouts, systems engineered to reduce installation time without sacrificing quality or compliance. The most practical response is designing electrical systems that work with the workforce available, not against it.
What this means for builders
Homes now require smarter, safer, and more flexible electrical infrastructure than ever before. These four forces, codes, loads, safety, and labor, are making the electrical system one of the most consequential design decisions in residential construction. The decisions being made now will shape how homes perform for decades.
Learn more
For a deeper dive into how these forces are reshaping residential construction – including practical solutions for managing increased loads, ensuring safety compliance, simplifying installation, and working within labor constraints – download our whitepaper.
For more insights on how ABB can help you with your next residential product, Residential | ABB Electrification U.S.
Sources:
1. https://www.nfpa.org/education-and-research/electrical/nec-enforcement-maps
2. https://solartechonline.com/blog/average-household-power-consumption-guide-2025/
3. https://www.nerc.com/globalassets/our-work/assessments/2024-ltra_corrected_july_2025.pdf