ABB to supply drive system for Guangxi Jianhui’s planned large-scale paper production line

ABB to supply drive system for Guangxi Jianhui’s planned large-scale paper production line

  • ABB will deliver an integrated drive system solution for Guangxi Jianhui Paper’s PM8 production line
  • Once operational, the paper machine is expected to become Asia’s largest extensible bag paper production line
  • Advanced automation and drive technologies will support efficient, reliable and low carbon paper production

ABB has signed an agreement with Guangxi Jianhui Paper Co., Ltd. to supply a comprehensive paper machine drive system for the company’s PM8 production line as part of its integrated forestry-pulp-paper project in Guangxi, China. Scheduled for commissioning in the fourth quarter of 2026, the new line is expected to become the largest extensible bag paper production line in Asia1.

The project is a further step in the cooperation between ABB and Guangxi Jianhui, which previously included other ABB drive technologies, as the company expands production capacity to meet growing demand for high-end packaging paper products2.

As a key production base of Jianhui Group, Guangxi Jianhui’s integrated forestry-pulp-paper project is a major industrial development in the Guangxi Zhuang Autonomous Region. Launched in October 2023, the project is planned to deliver annual pulp and paper production capacity of 3.672 million metric tons. Two packaging paper production lines are already in operation at the site.

  • Guangxi Jianhui plans to further expand with four additional high-standard paper machine production lines on site in the future. Image Guanxi Jianhui
  • The mill's new line is expected to become the largest extensible bag paper production line in Asia. Image Guanxi Jianhui
  • PM8 will benefit from precise motor control and strong performance under dynamic and low-speed operating conditions. Image Guanxi Jianhui

The PM8 line currently under construction has been designed to combine high production efficiency with intelligent and energy-efficient manufacturing technologies. ABB’s scope of supply includes its PMC800 paper machine drive control system, ACS880 multidrives and low-voltage AC motors, together with engineering support, installation guidance and commissioning services.

“This project demonstrates how advanced electrification and automation technologies can help paper producers improve productivity, energy efficiency and operational reliability,” said Wilson Monteiro, Global Business Line Manager, Pulp, Paper and Fiber, in ABB’s Process Industries division. “We are pleased to support Guangxi Jianhui in building a modern, intelligent production line that strengthens its competitiveness in the high-end packaging paper market.”

ABB’s drive system solution was selected based on its ability to support stable, high-performance operation while reducing maintenance complexity and lifecycle costs.

The supplied solution includes ABB’s Direct Torque Control (DTC) technology, enabling precise motor control and strong performance under dynamic and low-speed operating conditions. The drive system is also designed with simplified cabinet structures to support easier maintenance and improved serviceability.

To enhance long-term operational reliability, the PM8 system will use fiber-optic communication technology and dedicated maintenance networks to reduce the risk of downtime caused by electromagnetic interference. Original du/dt filters are also included to help extend motor insulation lifetime and minimize shaft currents.

The system has been designed to meet stringent industrial safety requirements, including Performance Level e (PL e) safety functions. ABB’s paper industry-specific control software will provide operators with an intuitive user interface and preconfigured process libraries to simplify operation, reduce training requirements and support stable production performance.

“ABB combines strong technology expertise with deep understanding of the pulp and paper industry,” said Ran Hu, Deputy General Manager, Guangxi Jianhui Paper. “The PM8 project is an important milestone in our development strategy, and ABB’s solutions will help us build a highly efficient, intelligent and future-ready production line.”

Guangxi Jianhui plans to further expand the site with four additional high-standard paper machine production lines in the future. The successful implementation of PM8 is expected to create a strong foundation for continued collaboration between the two companies.

1. 广西建晖纸业有限公司林浆纸一体化项目PM7&PM8造纸车间及配套桩基工程正式开工!-东莞建晖纸业有限公司|林浆纸一体化大型造纸企业|涂布白板纸·牛皮箱板纸·绿色循环制造

2. A Comprehensive Review of the Pulp, Paper, and Forest Products Industry in 2025

ABB is a global technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. By connecting its engineering and digitalization expertise, ABB helps industries run at high performance, while becoming more efficient, productive and sustainable so they outperform. At ABB, we call this ‘Engineered to Outrun’. The company has over 140 years of history and around 110,000 employees worldwide. ABB’s shares are listed on the SIX Swiss Exchange (ABBN) and Nasdaq Stockholm (ABB). www.abb.com

ABB’s Automation business automates, electrifies and digitalizes industrial operations that address a wide range of essential needs – from supplying energy, water and materials, to producing goods and transporting them to market. With its ~26,000 employees, leading technology and service expertise, Automation helps process, hybrid and maritime industries outrun – leaner and cleaner. go.abb/automation

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp