Zurich, Switzerland, June 22, 2016 - ABB technology products - low-voltage switchgear, motor-controller, electrical panels and automated lighting systems - will be used to power the factory's entire electrical system. The project includes the supply of Emax 2, the world's first combined circuit breaker and power manager, which uses 25 percent less copper than traditional circuit breakers and can improve energy efficiency by up to 20 percent.
"Now more than ever, energy efficiency is a major factor not only in our end product, but also all along our value chain," said Ryoji Kurosawa, COMPAS chief executive officer. "Working with ABB's solutions helps us to achieve those goals throughout our production line."
Renault-Nissan and Daimler have stated that they intend to produce 1.1 million vehicles per year at their new Mexican factory. According to news reports, the Mexican car industry showed a 5.6 percent increase from 2014 to 2015, with the production of 3.4 million cars and light trucks, in the face of robust demand.
"We at ABB are proud to provide our technological breakthroughs and expertise to Nissan and Daimler as they reduce the factory's carbon footprint, improve energy efficiency and protect people and equipment," said Tarak Mehta, president of ABB's Electrification Products division. "This project supports our Next Level strategy focus on driving industrial productivity improvements and reducing energy consumption."
The Aguascalientes factory's electrical system includes Emax 2 circuit breakers; Tmax Link distribution boards; the TVOC-2 arc guard system; and an automated lighting solution, the new ABB i-bus® KNX system.
The motor-control centers are integrated through System pro E power technology to safeguard personnel against electrical short circuits and to keep the system running with maximum efficiency and minimum maintenance and downtime.
ArTu "L", the automated lighting panel integrates the new ABB i-bus® KNX system that meets the highest requirements for applications in modern home and building control and is based on the proven KNX technology. ABB i-bus® KNX is a system supported by building controllers (lighting, sun protection, heating, ventilation and air conditioning) and intelligent networks that contributes significantly to the optimization of energy consumption, simplification of building monitoring and maintenance.
ABB (www.abb.com) is a leading global technology company in power and automation that enables utility, industry, and transport and infrastructure customers to improve their performance while lowering environmental impact. The ABB Group of companies operates in roughly 100 countries and employs about 135,000 people.