Industrial operators preparing for the U.S. Department of Energy's 2027 motor efficiency requirements now have a simple, yet advanced, solution with ABB's new SD200 SP4 severe-duty motor. Designed for maximum compatibility with existing SD200 motors, the SD200 SP4 delivers NEMA Premium® 4 efficiency while simplifying upgrades, reducing energy consumption and minimizing supply chain complexity.
Beginning June 1, 2027, manufacturers will no longer be permitted to produce 100-250 horsepower motors that meet current NEMA Premium efficiency standards. Companies that delay upgrading risk longer lead times, limited product availability, last-minute redesigns and higher project costs as demand for compliant motors increases.

"ABB’s SD200 SP4 gives customers a proven, practical path to DOE compliance today before market pressure builds," said Courtney Pickett, Product Specialist, ABB NEMA Motors. "Operators can transition to higher efficiency without redesigning applications, helping ensure compliance while keeping operations running."
Built on ABB's SD200 severe-duty platform, the motor features heavy-duty cast iron frames, C-4140 high-strength steel shafts, Class H insulation systems and IP55 ingress protection for demanding environments, including mining, chemical processing, petroleum refining, pulp and paper, water and wastewater.
SD200 SP4 combines NEMA Design B performance with rugged severe-duty construction to increase energy performance without compromising reliability. Compared to NEMA Premium motors, it reduces motor losses by an average of 20 percent, lowering electricity consumption in continuously running applications. SD200 SP4’s reduced heat generation also supports cooler operation, longer service intervals and dependable long-term operation.
Because ABB’s SD200 SP4 is fully frame-by-frame compatible with existing SD200 motors, operators can replace motors without costly equipment redesigns. Drop-in compatibility streamlines specification, installation and maintenance, while an oversized conduit box wiring access and serviceability.
SD200 SP4 is available now in 125-250 horsepower two- and four-pole configurations through ABB's authorized distribution network. Six-pole configurations within the same horsepower range will be available later this year.

Learn more about ABB's SD200 severe-duty motors at abb.com.
ABB Motion, a global leader in motors and drives, is at the core of accelerating a more productive and sustainable future. We innovate and push the boundaries of technology to contribute to energy efficient, decarbonizing and circular solutions for customers, industries and societies. With our digitally enabled drives, motors and services we support our customers and partners to achieve better performance, safety and reliability. To help the world’s industries outrun - leaner and cleaner, we deliver motor-driven solutions for a wide range of applications in all industrial segments. Building on more than 140 years of domain expertise in electric powertrains, our more than 23,000 employees across 100 countries learn and improve every day. go.abb/motion
ABB is a global technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. By connecting its engineering and digitalization expertise, ABB helps industries run at high performance, while becoming more efficient, productive and sustainable so they outperform. At ABB, we call this “Engineered to Outrun.” The company has more than 140 years of history and around 110,000 employees worldwide. ABB’s shares are listed on the SIX Swiss Exchange (ABBN) and Nasdaq Stockholm (ABB). www.abb.com