ABB emergency lighting solution selected for 2026 IES Industry Progress Report

ABB emergency lighting solution selected for 2026 IES Industry Progress Report

  • EUPHR Series and LAPHR Series Egress Luminaires selected for the IES Industry Progress Report, which highlights significant advancements in the art and science of lighting
  • Designed for high-ceiling industrial facilities, asymmetric optics provide clear, highly uniform illumination along emergency exit routes at mounting heights of up to 70 feet
  • Wide spacing between luminaires can reduce the number of units required while centralized emergency power simplifies maintenance

ABB’s EUPHR Series and LAPHR Series Egress Luminaires, designed to illuminate paths of egress, or emergency exit routes, have been selected for inclusion in the 2026 Illuminating Engineering Society (IES) Industry Progress Report. Published annually, the report highlights significant advancements in the art and science of lighting. Submissions are assessed through an impartial judging process based on their uniqueness, innovation, and significance to the lighting industry.

The EUPHR Series and LAPHR Series Egress Luminaires provide clear illumination along emergency exit routes in high-ceiling industrial environments such as warehouses, manufacturing plants, and distribution centers, where conventional emergency lighting can struggle to provide effective coverage.

The luminaires feature a purpose-built photometric system combining fixed asymmetric optics, 355-degree rotational flexibility for precision aiming, and adjustable multi-head LED modules. These features enable light to be directed precisely along the path of egress, providing highly uniform illumination and reducing dark or unevenly lit areas that could make it harder for people to find their way out of buildings safely.

center

Designed for mounting heights of up to 70 feet, individual luminaires can be positioned up to 192 feet apart depending on the configuration, while maintaining consistent illumination along the exit route. By allowing wider spacing between luminaires, the system can reduce the number needed across a facility, offering greater design flexibility while helping to lower equipment and installation costs.

The Egress luminaires operate as part of a centralized mini-inverter system, which provides backup power to the emergency lights if the building’s normal electricity supply fails. A single mini-inverter can support up to 81 luminaires. The centralized system also provides convenient floor-level access, making the system easier to service while helping to reduce ongoing maintenance costs.

“Emergency lighting in industrial buildings with very high ceilings comes with a distinct set of challenges,” said Fabio Mercurio, Business Line Leader for Emergency Lighting at ABB Electrification’s Smart Buildings Division. “People still need a clear route out, but providing effective coverage across such large spaces can be difficult.”
“The EUPHR Series and LAPHR Series Egress Luminaires were developed to provide the precise, uniform illumination these spaces require and to make emergency lighting systems simpler to design and maintain. Inclusion in the IES Industry Progress Report is an important recognition of the engineering behind the solution and its practical value for facility owners and operators.”

The 2026 IES Industry Progress Report was presented at IES26: The Lighting Conference and will be published in the November issue of LD+A Magazine.

The recognition follows the introduction of the EUPHR Series and LAPHR Series Egress Luminaires to the North American market in April 2026. For more information, visit: EUPHR Series and LAPHR Series.

 

About ABB
ABB is a global technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. By connecting its engineering and digitalization expertise, ABB helps industries run at high performance, while becoming more efficient, productive and sustainable so they outperform. At ABB, we call this ‘Engineered to Outrun’. The company has over 140 years of history and more than 110,000 employees worldwide. ABB’s shares are listed on the SIX Swiss Exchange (ABBN) and Nasdaq Stockholm (ABB). www.abb.com

About ABB Electrification

ABB Electrification is a global technology leader enabling the efficient and reliable distribution of electricity from source to socket. With more than 50,000 employees across 100 countries, we collaborate with our customers and partners to solve the world’s greatest challenges in electrical distribution and energy management. As the energy transition accelerates and electricity demands grow, we are electrifying the world in a safe, smart and sustainable way. At ABB, we are engineered to outrun, and we are passionate about helping our customers and partners do the same. go.abb/electrification

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp