ABB launches digital platform for optimizing operation of water networks

  • AquaMaster+™ delivers crucial insights that will help water utilities prevent pipeline water losses and optimize operations
  • Fleet and device level insights support water network operators with more efficient resource management
  • The digital service is available to water companies using ABB’s AquaMaster4™ flowmeters or as a standalone software solution

ABB has launched AquaMaster+™, a digital platform for smart water network management, designed to help water utilities monitor, analyze and manage their water networks, preventing pipeline water losses and optimizing operations. The integrated platform includes hardware, advanced software capabilities, and cloud-based decision-making tools. The service is available to water companies using ABB’s AquaMaster4™ flowmeters or as a standalone software solution that can be integrated into existing systems.

“With pressure mounting on water resources globally, a great deal of work is done to prevent losses in the distribution system and to help save water through more efficient resource management,” said Raghu Kumar NV, Global Product Manager, ABB’s Measurement & Analytics division. “AquaMaster+ will enable this work by connecting water utilities to crucial flow measurement insights from their AquaMaster4 or other devices, helping the water sector outrun – leaner and cleaner.”

AquaMaster+ offers fleet level insights that include fleet overview with GIS mapping, as well as device insights that cover flow and pressure shifts, device diagnostics, and remote configuration.

The possibility for remote configuration and management improves response times and reduces travel costs, while real-time monitoring enables proactive issue detection and response. 

As it stores device and generic event logs, AquaMaster+ allows for comparison of parameters such as flow rate and pressure, helping water utilities identify anomalies early.

With the possibility of adding virtual flowmeters, AquaMaster+ allows for modeling and comparison of scenarios, simulating real situations and their outcomes, and ultimately allowing operators to make better decisions.

The platform offers intuitive navigation, with minimal training required, reducing the possibility for human errors and enabling quick access to critical information.

ABB’s AquaMaster flowmeters measure water flow in real time, tracking the exact quantities of water passing through the water network. The flowmeters offer measurement accuracy down to flow velocities lower than 0.1m/s and detect leaks faster than many conventional solutions.

In 2022, AquaMaster4 Mobile Comms became the world’s first electromagnetic flowmeter with bidirectional connectivity. With over 50 years in the water industry, ABB offers one of the most comprehensive water management and water analysis portfolios on the market.

  • AquaMaster+ in operation
  • AquaMaster+ is a digital platform for smart water network management
  • AquaMaster+

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp