It’s a situation many panel builders recognize: a project is moving forward, the specification is locked, and then reality sets in. A component is not available, lead times don’t align, or a more practical alternative becomes obvious - but the approved brand list leaves no room to adjust.
Within tightly defined project specifications, consultants and end users frequently lock in approved vendors, limiting flexibility from the start. While this helps ensure consistency, it can also introduce unnecessary constraints during design and execution.
In practice, not all specifications reflect the most efficient or practical solution. Equivalent components may offer the same performance, better availability, or improved cost efficiency. However, proposing alternatives is rarely straightforward. It requires not only technical knowledge but also the ability to build a convincing case.
A key challenge is gaining acceptance. Consultants typically expect clear technical justification, documented equivalence, and assurance that performance and compliance will not be affected. Without this level of detail, even well-founded proposals are often rejected.
At the same time, panel builders need to manage risk throughout the project life cycle. Changes introduced during design, testing, or commissioning can create uncertainty if drawings, configurations, or documentation are not fully aligned. Small inconsistencies can quickly lead to delays or rework.
This is where strong technical backing becomes critical. Access to technical documentation, product information, and relevant expertise can help when proposing alternatives or resolving issues, including identifying equivalent solutions that meet project requirements without introducing additional risk. When questions arise during factory testing or commissioning, access to technical expertise and relevant information can help keep projects moving.
Clear guidance and practical tools also play an important role. Well-structured configurators, reliable documentation, accurate drawings, and consistent specifications reduce the risk of errors and make it easier to implement changes correctly.
Navigating specification-driven projects is not about pushing substitutions for the sake of it. It is about making well-informed decisions that balance performance, availability, and project requirements. With the right support, panel builders can increase flexibility, reduce delays, and deliver projects more efficiently.
To learn more about how structured partner support, tools, and programs can help address these challenges, explore our medium-voltage channel partner resources.

About the author
Marco Guarneri works closely with channel partners, OEMs, and panel builders within ABB's medium-voltage business. He focuses on topics related to switchgear applications, project requirements, and partner development.