ABB enables grid resilience: Standardized infrastructure for decentralized generation

ABB enables grid resilience: Standardized infrastructure for decentralized generation

Germany's renewable energy growth demands grids that balance generation, manage congestion, and maintain stability. ABB's standardized solutions enhance grid resilience and enable reliable renewable integration at scale—proven by the Ahlerstedt-Oersdorf battery energy storage project, where modular systems accelerate deployment and reduce costs.

From grid volatility to scalable solutions

According to the German Federal Network Agency, renewable electricity generation reached nearly 59% in 2025 [1], advancing toward the 80 percent target by 2030. However, this introduces a structural challenge: generation from wind and solar is volatile and weather-dependent. Demand volatility is also rising, driven by new high-power consumers like charging stations and data centers, emerging across all grid levels.

As generation shifts from centralized power plants to decentralized, weather-dependent assets, the electricity grid must adapt. Grid stability can no longer rely solely on generation following demand. As a result of this grid evolution, flexibility must be embedded directly into the infrastructure. Battery energy storage systems are one emerging market solution that is also able to operate bidirectionally. They absorb surplus electricity during peaks in wind or solar generation and release it when demand rises or generation drops. Through peak shaving and load-shifting, they stabilize grids, prevent renewable curtailment, and ensure supply security. 

Across various scenarios, Germany’s Federal Network Agency projects a storage power requirement of around 130 to 180 GW by 2040 [2] — approximately seven to eleven times the 2025 level. Meeting this demand requires new approaches to planning and executing battery storage projects that enable faster, cost-effective rollout with consistent quality. 

Standardization as an enabler for scale

To meet Germany's projected storage demand, battery projects need to be deployed faster, more consistently, and at lower cost. Yet many installations continue to be engineered as bespoke projects, increasing complexity, extending timelines, and limiting scalability. 

ABB addresses this challenge through standardized, prefabricated infrastructure solutions that simplify design, reduce on-site work, and accelerate deployment. By combining modular containerized substations, medium-voltage switchgear, transformers and protection systems into factory-tested solutions, projects can move from design to commissioning more efficiently and with greater consistency. 

The value of this approach is already being demonstrated in real-world battery storage projects. One example is the Ahlerstedt-Oersdorf installation in northern Germany, where ABB and be.storaged worked together to deliver a scalable and efficient grid connection solution.

From concept to reality in northern Germany

Northern Germany's decentralized renewable energy is accelerating due to strong wind and expanding solar capacity. Peak production often exceeds local demand, making battery storage systems essential for absorbing surplus power and maintaining grid stability. 

be.storaged GmbH, a subsidiary of EWE AG, delivers energy storage solutions for utility-scale, commercial, and industrial applications. Founded in 2017, the company combines technical expertise with extensive market experience. In Ahlerstedt-Oersdorf, be.storaged partnered with Terra One to develop a 15 MW / 30 MWh battery energy storage system. Covering around 1,300 m², the installation can store enough energy to supply approximately 2,500 households for one day.

A challenge shaped by compatibility and speed

To connect the battery storage seamlessly to the grid, be.storaged required a compact medium-voltage distribution solution with a minimal number of interfaces. The remote location of the site created additional requirements for durability, simplified logistics, and a footprint that avoided heavy civil works or oversized cranes. Speed was equally critical. The distribution solution needed to align precisely with the battery commissioning schedule. This made a pre-engineered, factory-tested, ready-to-connect approach essential, supported by an experienced project partner capable of meeting tight timelines.

ABB’s solution in practice

ABB supplied four EcoFlex container stations tailored to the specific demands of the Ahlerstedt-Oersdorf project. Based on modular, pre-engineered configurations, EcoFlex combines electrical performance, robust outdoor design, and optimized footprint. Each container was delivered fully assembled and routine-tested at the factory, reducing on-site work and coordination effort. 

Inside the containers, ABB integrated SafePlus 24 kV medium-voltage switchgear, a project-engineered low-voltage distribution board, and a 4.4 MVA distribution transformer. This configuration delivered a coordinated and reliable distribution setup aligned with the battery system's requirements, while reducing the need for secondary switchgear by around 40 percent compared to conventional layouts. With a delivery time of just 31 weeks, the EcoFlex containers guaranteed maximum planning certainty for the entire project. This included supply of major components (transformer and RMU), transport from Vietnam, and customs clearance in Germany.

"ABB provided us with solutions to the challenges we faced on the Ahlerstedt-Oersdorf project: proven technology within our budget and ready for operation sooner than anticipated. What truly sets ABB apart is its in-depth understanding of projects and its exceptional consulting services – a rare combination. This valuable partnership marks the beginning of a promising and fruitful collaboration.”
Kevin Hendzlik, Team Lead-Supplier Management be.storaged GmbH
  • EcoFlex container stations for the Ahlerstedt-Oersdorf battery energy storage system
  • Fully assembled, factory-tested EcoFlex Container station
  • Ahlerstedt-Oersdorf battery energy storage system by be.storaged and Terra One

Results and outlook

With the EcoFlex containers in place, be.storaged achieved full compatibility between its battery technology and the local grid. The solution provided a high-power-density connection, reduced coordination effort, and the use of secondary switchgear, thereby lowering logistical and construction requirements. During project execution, ABB’s project management team in Germany enabled quick responses to on-site challenges. 

The Ahlerstedt-Oersdorf installation demonstrates how standardized, prefabricated distribution solutions can turn battery storage from an engineering challenge into a scalable infrastructure element. be.storaged and ABB continue their partnership in an increasing number of follow-up projects. ABB's solution not only accelerates individual projects – it also makes it possible to meet the massive demand in Germany for battery storage capacity by 2040. 

By enabling faster, more repeatable deployment of battery storage systems, ABB’s standardized, prefabricated solutions support Germany’s growing need for energy storage capacity and contribute to a more flexible and resilient power grid.

Sources

[1] Source: German Federal Network Agency, “Federal Network Agency publishes data on the 2025 electricity market,” German press release, 5 January 2026, https://www.bundesnetzagentur.de/1087156


[2] Source: German Federal Network Agency “Scenario Framework for the Electricity Grid Development Plan 2040/2045”, June 2026, Szenariorahttps://www.bundesnetzagentur.de/DE/Fachthemen/ElektrizitaetundGas/NEP/DL_Szenariorahmen/2027/SR_Entwurf2027Strom.pdf?__blob=publicationFile&v=2hmen 2026  

Fact box

ABB's delivery

  • Four EcoFlex container stations
  • Integrated SafePlus 24 kV medium-voltage switchgear
  • Integrated project-engineered low-voltage distribution board
  • Factory-tested, pre-assembled delivery
  • Compact footprint for simplified logistics

Customer snapshot

be.storaged GmbH offers comprehensive energy storage solutions for both the utility-scale segment and the commercial and industrial sector. The company provides end-to-end support for projects—from development through planning and construction (full EPC) to operation and maintenance. With okean, be.storaged has developed its own energy management system that uses intelligent algorithms to flexibly control energy flow with AI support. Since its founding in 2017 as a subsidiary of EWE AG, be.storaged has combined technical expertise with years of market experience to create sustainable, flexible energy management systems.

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp