ABB has expanded its all-compatible drives offering to include the ACS6080 medium voltage (MV) drive for critical applications. The new drive introduces a breakthrough control technology, developed by ABB, that brings high performance motor control to demanding processes used in industries such as mining, metals and marine. The drive also enables plants to operate more efficiently and produce higher quality output.

Traditionally, achieving high dynamic performance and excellent power quality needed hardware with multiple devices. However, this increase in components could decrease reliability of the equipment. The ACS6080 drive maintains the same highly reliable hardware as its predecessor, the ACS6000, and includes the new advanced control capability, known as Model Predictive Pulse Pattern Control (MP3C).
ABB’s MP3C technology combines model predictive control with optimized pulse pattern to modulate the semiconductors. This means that at every point in time this control can anticipate the best motor operation point by finding the perfect compromise between dynamics, efficiency and harmonic distortion.
The new control enables system integrators and plant operators to maintain stability, while reducing investment and operational costs by using a smaller drive or a smaller motor. The increased power capability of the ACS6080’s single power module reduces the footprint of the drive by up to 20 percent. The new control helps to reduce operational cost in two ways: it is more energy efficient than other control solutions, and maintenance costs are reduced as there is less mechanical and thermal stress on the equipment leading to longer lifetime of the components.
The ACS6080 provides extensive input/output connectivity and supports all major fieldbus protocols, making it easy to integrate into existing systems and processes. It is compatible with ABB Ability™ condition monitoring services, allowing customers to obtain real-time data about the status and performance of the monitored equipment from any location.
“The ACS6080 MV drive provides benefits which help deliver exceptional value to industrial processes in terms of product quality, uptime, safety and energy efficiency,” says Ester Guidi, Product Manager, ABB Drives.
The new drive delivers a high level of safety for people and equipment via an arc-resistant design and certified functional safety features. The ACS6080 is built on ABB’s common drive architecture, enabling a faster and harmonized startup, commissioning and monitoring. Once a user has learned how to use one all-compatible drive, they can then operate any other drive in ABB’s all-compatible offering.
The modular design of the ACS6080 enables it to be configured for single or multi-motor applications. It controls all types of AC motors including induction, synchronous and permanent magnet, without the need for different software. The ACS6080 can be tailored to any heavy industrial application, and has a power range from five megawatt (MW) to 36 MW.
ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in electrification products, robotics and motion, industrial automation and power grids, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner of Formula E, the fully electric international FIA motorsport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 135,000 employees. www.abb.com