Release of IED Connectivity Package version 8.3 for Relion® REB500 series

center

JUNE 19TH, 2019

We are pleased to announce the release of IED Connectivity Package version 8.3 for the Relion REB500 series.

New features and benefits

This new version of the IED Connectivity Package for Relion REB500 series enables the interaction between the Relion REB500 series version 8.3 IEDs and the protection and control IED manager PCM600 version 2.7 or later.

The new connectivity package enables support for the following features in PCM600 version 2.7 and Relion REB500 series version 8.3:

  • Windows 8 and 10, with native 32-bit and 64-bit support
  • Support for PCM600 64-bit
  • Read/write of configurations
  • Online IED configuration revision comparison
  • IEC 61850 Ed 2 support
  • Cyber security (read of security events)

Read all about this release in the Release note and the Read me file.

Kind regards,
Krister Hagman, Global Product Manager

Contact us

Share this article

Facebook LinkedIn X WhatsApp