According to Mr. Franco Vecchiato, ABB South East Asia Sales & Marketing Manager, MCCB Tmax XT has advantages for it simple look, complying with IEC 60947-2 standards, smarter design, and competitive price.
In these seminars, LP also introduced the Current Measurement System (CMS) that helps to increase the ability to monitor energy system with various functions such as exactly detecting power failure, early warning on abnormally operations, and warning to avoid unwanted trip system caused by overload in every single circuit. CMS can manage the energy consumption level by recording or checking actual value of current, helping customer to use energy more efficiently and to plan energy saving in the future.

The last new product introduced in seminars was soft-starter PSE - efficiency range that can be applied to start many types of load such as fan, conveyor, compressor… especially for pump applications in water supply and waste water treatment system.

The seminars attracted about 250 participants from distributors, electrical contractors, engineering contractors, consultant companies and other industrial manufacturers, of which many showed the interest in long term cooperation with ABB.