ABB is launching its DC Wallbox for electric vehicle (EV) charging at the Cenex LCV event at Millbrook, Bedfordshire on 4 to 5 September 2019.

The DC Wallbox was developed for offices, dealerships and public parking places, where it will provide direct current (DC) that offers a shorter charging time than a conventional alternating current (AC) device. With an output of 24 kilowatt (kW), it is compatible with all existing 500 V battery EVs, as well as the next generation of high-voltage vehicles. Depending on the vehicle, it can have drivers topped up and back on the road within 1-3 hours.
Connectivity is key to success in EV charging. Featuring ABB Ability Connected Services, the DC Wallbox enables authentication, payment, monitoring, remote diagnostics and repair, as well as wireless updates and upgrades.

ABB is also showcasing its Terra HP (high power) charger, which can add a range of 124 miles in only eight minutes, making it the world’s fastest charger. It was launched to the UK market at Cenex LCV in 2018 and was developed to overcome range anxiety in EV charging.
In addition, a Jaguar I-PACE e-TROPHY car will form the centrepiece of the stand thanks to ABB’s title partnership of the ABB FIA Formula E championship. The Jaguar I-PACE e-TROPHY is the main feeder racing series for ABB Formula E.
Oliver Johnson, ABB’s business development manager for EV charging, said: “The new DC Wallbox will support greater adoption of e-mobility by private vehicle owners and businesses alike. ABB's DC charging infrastructure offers reliable fast charging along with digital connectivity.”
With more than 11,000 DC fast chargers sold across 76 countries world-wide, ABB is a global leader in DC fast charging.
ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader with a comprehensive offering for digital industries. With a history of innovation spanning more than 130 years, ABB is today a leader in digital industries with four customer-focused, globally leading businesses: Electrification, Industrial Automation, Motion, and Robotics & Discrete Automation, supported by its common ABB Ability™ digital platform. ABB’s market leading Power Grids business will be divested to Hitachi in 2020. ABB operates in more than 100 countries with about 147,000 employees. www.abb.com
— | ||
Media Relations | ABB Ltd | |