Sarawak is on course to become a developed state with a high-income economy by 2030. Fueled by its digital transformation agenda and the Sarawak Corridor of Renewable Energy (SCORE), the State has drawn significant investments from energy intensive industries, resource-based industries, halal products and ecotourism. In its bid to balance economic growth and improved quality of life for rural communities, Sarawak has set out to achieve full electrification by 2025.
Strategies deployed to accelerate and revolutionize rural electrification include normal distribution through the Rural Electrification Scheme extension; transmission extension through the Rural Power Supply Scheme as well as standalone renewable hybrid and the internationally recognized Sarawak Alternative Rural Electrification Scheme or SARES. However, access to electricity for remote communities remains a challenge due to extreme rugged terrain and sparse population.
Electricity is typically provided by diesel-powered generators, which are expensive to operate and maintain for low-income communities in remote villages. Diesel has to be transported over long distances either by river or roads, and during the wet season the price of diesel increases due to limited or uncertain supplies caused by disrupted road access.

To this end, the MGS100 offers a sustainable and cost-effective solution to reduce dependence on fossil fuels while cutting operational costs. The system is formed from an integrated solar PV and battery energy storage converter with an additional AC input. This can incorporate either biofuel or diesel generation, or even an existing grid connection into the microgrid's energy mix.
Built to perform in extreme environments, the system offers remote monitoring capabilities, making vital diagnostics available while its modular design eases maintenance. In addition to this, the battery input means that once batteries are connected, power can be delivered even after dark, minimizing fuel consumption.
The MGS100 made its debut at the 4th International Sustainable Energy Summit (ISES) in Kuching today. Themed 'Sustainable Energy: The Future is Here', the summit focuses on two topics namely the future role of block chain in the energy market and the emergence of energy storage systems.
"We are thrilled to be able to introduce the MGS100 today. As a pioneering technology leader, ABB delivers innovative solutions to meet our customers' most complex challenges. I'm confident that the MGS100 will be able to reinforce our position as a partner of choice for making affordable, safe and reliable electricity supply a reality for remote communities in Sarawak," said Jukka Poutanen, Managing Director, ABB Malaysia Sdn Bhd.
ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in electrification products, robotics and motion, industrial automation and power grids, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner of Formula E, the fully electric international FIA motorsport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 135,000 employees. www.abb.com
ABB's history in Malaysia began when the first power generator was installed in 1904. ABB Malaysia currently employs around 620 professionals. It is a regional switchgear hub for medium voltage switchgear, low voltage switchgear and motor control centers serving key markets such as Southeast Asia, New Zealand, Australia and Japan.
-
For more information please contact:
| Nirmala Devi Phone: +603 5628 4888 Email: nirmala.devi@my.abb.com |
ABB Malaysia Sdn Bhd Lot 608, Jalan Lagoon Selatan Bandar Sunway 47500 Subang Jaya, Selangor Malaysia Tel: +603 5628 4888 Fax: +603 5632 7889 |