ABB supports Denza 500 in sustainable pilot on Roof of the World

Safe, reliable and stable operation of ABB DC chargers on the Qinghai-Tibet Plateau ensures the continuous running of electric vehicle pilot

center

From April 2 to 15, 2018, a test drive of Denza 500 pure electric vehicles was held in the Lhasa-Linzhi section of China National Highway 318 on the Qinghai-Tibet Plateau, aptly named the 'Roof of the World' due to its 3500m elevation. As the global strategic partner, ABB provided the DC charger for this test drive, ensuring the safe, reliable and smooth operation of the pilot.

Due to restrictions on the development of new energy vehicles and supporting charging infrastructure facilities in Tibet, no public charging stations had been built before. Therefore, the ABB DC chargers used for this test drive were transported from Shenzhen and installed around the Shangri-La Hotel, Lhasa.

The charger comes with ABB Ability™ connected solutions, which increase visibility and control of infrastructure networks, while minimizing downtime and increasing efficiency. ABB Ability™, which is ABB's unified, cross-industry digital offering, delivers web-enabled connectivity that allows network operators to monitor and configure the charge points from any location. Driver issues can be resolved remotely and equipment can be serviced with minimal downtime. It offers flexibility to connect to any charging network, back-office or energy management solution.

Frank Mühlon, Head of ABB's Global Business for Electric Vehicle Charging commented: "We are delighted to have been selected as a partner for this test drive, which has delivered very positive results. According to the charging data fed back from the field, the performance of ABB DC chargers was the same in the plateau area as in the plains, with no slowdown, interruption, or instability resulting from the elevation and associated harsh conditions."

There are two types of charging methods currently available to EV owners in Lhasa: one is to install an AC charger where the vehicle is parked; the other is use 'random charging', which requires a long charging time and involves a certain safety risk, with charging cables lowered down to the parked vehicle from a nearby building.

The solution from ABB offers a safer and more efficient alternative. The pre-charging protection, active self-test, interlocking mechanism, temperature and humidity sensing management features of ABB DC chargers, if used, will improve the safety of charging, and the charging process can be completed within 1-2 hours.

The quality power resources and unique solar energy resources in Tibet provide natural conditions, which complement truly sustainable transport. ABB's new green charging ecology (photovoltaic + energy storage + charging) integrates advanced technologies such as photovoltaic power generation, large-capacity energy storage batteries, and smart chargers, which provide comprehensive infrastructure solutions and technical support for the promotion and popularization of electric vehicles, as well as a new option for the protection of the pure land of the Qinghai-Tibet Plateau.

At present, charging infrastructure is only in its early days of implementation in Tibet. However, the country has already promoted the construction of charging infrastructure in public areas and communities, with ABB poised to provide more extensive services to enable sustainable mobility across Tibet.

ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in electrification products, robotics and motion, industrial automation and power grids, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner of Formula E, the fully electric international FIA motorsport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 135,000 employees. ABB has a full range of business activities in China, including R&D, manufacturing, sales and services, with 17,000 employees located in 139 cities, 40 local companies, and online and offline channels across over 300 cities.

-
For more information please contact:

Natalie Hodges

ABB Ltd
Media Relations Manager Affolternstrasse 44
Electrification Products Division
Phone: +41 (0)43 317 54 04
E-mail: natalie.hodges@ch.abb.com
8050 Zurich
Switzerland


Please visit: http://new.abb.com/cn
ABB Digital Marketing Center: https://mall.abb.com.cn
Sina Weibo: @ABB Electrification Products
Official WeChat Account: cnabblp
Official WeChat QR Code:

center


Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp