ABB supplies central inverter solutions for two PV power plants in Jordan, totaling 102 MWac

ABB’s central inverter solutions were chosen to power photovoltaic (PV) solar power plants Mafraq I and Mafraq II. The two plants, located in Mafraq, Jordan, with a total AC power of 102 MW, will be constructed by Fotowatio Renewable Ventures (FRV)

ABB has signed contracts with FRV, a leading global utility-scale solar developer, for the supply of central inverter solutions to PV power plants Mafraq I and Mafraq II. The plants will be located in Mafraq, Jordan, which is one of the areas of the highest solar irradiation in the region. These construction projects were awarded in the second round of Jordanian solar program. The two plants, totaling 102 MW AC nominal rating, are expected to be operational summer 2018.

According to the newly signed contracts, the plants will be powered by ABB's central inverter solutions consisting of 62 pcs of 2 MVA outdoor type central inverters, 30 pcs of 4 MVA and 2 pcs of 2 MVA medium-voltage step-up stations. The stations are using ABB's outdoor type oil transformers and ABB's 36 kV SafeRing-type Ring Main Units delivered with outdoor enclosure. The grid code compatibility is secured by ABB's plant controller together with the inverters' advanced grid support features. Commissioning is also included in the delivery.

ABB has been present in the Middle East since 1920s. One of the corner stones of ABB success in the region is the experienced and wide service organization that can support projects like this for years to come. This delivery is a milestone for ABB in both the Jordan PV market and whole territory.

"We believe strongly in the potential of solar energy in this territory and are committed to further developing our capabilities to support our customers during the whole lifetime of their projects," says Anshuman T, head of ABB sales for solar inverters in the region.

"For FRV these two projects reflect the company's strong commitment to promoting the generation of clean and affordable energy in Jordan and enabling the country's sustainable development. ABB was selected as inverter supplier for these projects because of the high product performance and good local presence, which can support the solutions delivered over the lifetime of the project," says Carlo Frigerio, Managing Director of FRV in the Middle East.

About ABB
ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in electrification products, robotics and motion, industrial automation and power grids, serving customers in utilities, industry and transport & infrastructure globally. Continuing more than a 125-year history of innovation, ABB today is writing the future of industrial digitalization and driving the Energy and Fourth Industrial Revolutions. ABB operates in more than 100 countries with about 132,000 employees. www.abb.com

About FRV
FRV is a leading global solar development company with a project portfolio over 5GWdc in the emerging solar markets including Australia, the Middle East, Africa and Latin America. Since 2006, the management team has completed the construction, operation, maintenance and financing of over 780 MWdc of photovoltaic and CSP solar energy plants. Such projects represent more than US$ 2.5 billion in total financings with more than 20 leading banks. www.frv.com

For more information please contact:

Lynette Jackson
Head of Communications
Electrification Products Division
Affolternstrasse 44, P.O. Box
CH-8050 Zurich, Switzerland
Phone: +41 (0)43 317 54 04
E-Mail: lynette.jackson@ch.abb.com

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp