ABB will be in Intersolar South America, which will take place from August 22 to 24, in São Paulo, with launches for the renewable energy market. The multinational has been operating in the photovoltaic segment for more than 25 years and is a leader in the supply of equipment and solutions, with more than 26 GW of installed energy in more than 100 countries.
Renewables are expected to receive 3/4 of the $ 10.2 trillion that the world will invest in new forms of generation technology by 2040, according to Bloomberg New Energy Finance forecast. Brazil has more than 11,000 solar ceilings, most of them in homes and the expectation of the solar energy sector is to move R $ 4.5 billion in Brazil until December.
ABB has extensive portfolio of technologies for residential, commercial, industrial and microgrids applications, including solar inverters, transformers, low and medium voltage products, electrical protection, and predictive maintenance and monitoring systems. According to Bruno Monteiro, ABB Brasil's solar energy manager, the company brings three launches for this edition of the fair, which can be seen at the F8 booth.
"ABB is betting on the growth of this market and has new developments for residential facilities. One is the REACT inverter, with integrated storage, and the only one in Brazil that works with energy backup. The great advantage is that it offers autonomy and stability for the consumer, regardless of the power grid. If there is a blackout, the user can use the stored energy, "says the executive. "All generation information, with high level of detail, is sent via wireless via the device to the ABB platform in the cloud and the user has access via tablet or smartphone. Another solution that reinforces ABB's commitment to the Internet of Things, "adds Monteiro.
The company constantly invests in R & D to deliver high-performance technology solutions with added engineering value to customers. "Solar inverters already come with integrated protection, can be adapted to any type of installation and make the operator's life easier. ABB solutions deliver greater return on investment, delivering greater energy efficiency, reduced installation time and faster response times. "
ABB Releases:
REACT - Inverter with integrated storage for the residential market, available in 4.6 kW and 3.6 kW versions. It is equipped with a 2 kWh battery, which allows the backup of the energy generated for later use. The product offers energy self-sufficiency, aligns energy production with house consumption levels and can be managed remotely.
UNO-DM-PLUS - Inverter with focus on domestic installations. With compact design and high density, it has powers ranging from 1.2 to 5.0 kW. The wireless network of the product allows the installation to be done with the help of a smartphone in less than 5 minutes. It can be integrated with home automation systems, such as ABB-free @ home.
PVS-120 - Inverter for distributed generation applications (up to 120 kW). The product has the best density and power among the other options available in the market. Easy to install, it's compact and comes with built-in protections and reduces field work time. For servicing repairs and replacement of parts, simply unlock and lift the product's tip door.
Service:
Intersolar South America
Days: August 22 to 24
Hours: 12 a.m. - 8 p.m.
Estade: F8
Location: Expo Center Norte - São Paulo - SP
ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in electrification products, robotics and motion, industrial automation and power grids, serving customers in utilities, industry and transport & infrastructure globally. Continuing more than a 125-year history of innovation, ABB today is writing the future of industrial digitalization and driving the Energy and Fourth Industrial Revolutions. ABB operates in more than 100 countries with about 132,000 employees. www.abb.com