ABB’s new solar power storage solution, REACT 2, achieves 90 percent energy self-reliance

With its modular design, ABB’s new solar inverter with energy storage capability, REACT 2, provides a capacity of up to 12 kWh, increasing electric self-sufficiency of homes.

center

ABB's new REACT 2 inverter and energy storage solution includes a high-voltage Li-ion battery with a long life and a storage capacity of up to 12 kWh. The modular solution can grow with the needs of any household from 4 kWh to 12 kWh and significantly reduce electricity charges thanks to an achievable energy self-reliance of up to 90 percent.

The inclusion of a high-voltage battery (200 V) delivers more reliability and up to 10 percent more system efficiency compared to lower voltage alternatives (48 V).

Tarak Mehta, President, Electrification Products division at ABB said: "We know that prosumers want to harness energy and store it until needed. The growth in self-consumption is one of the most exciting trends in renewables, driving greater demand for integrated and efficient battery storage. We have responded to this with our new high-voltage solution, which not only delivers energy savings of up to 90 percent but will flex and grow as consumer demands change."

One of the advantages of REACT 2 is its modular design, which can be easily expanded from 4 to 8 to 12 kWh storage capacity to cope with the changing needs of any household, adapting as it grows and delivering double the maximum storage capacity of the first REACT model.

"It's this future-proof thinking incorporated into the design of REACT 2 that makes it ideal for energy efficient solar power storage. Further, the ability to install REACT 2 on both AC and DC sides, offers the perfect solution for new systems or the retrofitting of existing photovoltaic systems," added Mehta.
REACT 2 also offers complete installation flexibility, thanks to the different set-up configurations available. It is quick and easy to install with a simple 'plug and play' connection and an app for installers.

As demand for smarter energy solutions continues to grow, REACT 2 takes advantage of ABB's cloud-based, industry-leading portfolio of digital solutions, ABB Ability™, to provide home owners with complete control over their solar power usage.

Based on the combination of REACT 2 and ABB-free@home®, home owners can make the best use of the electricity generated by their photovoltaic system, avoiding consumption peaks by spreading the electricity load and keeping usage within the capacity of the energy harnessed.

REACT 2 transfers the information on solar energy, home consumption and battery status over a wireless network to the ABB-free@home system access point, which can then control other ABB-free@home devices including heating, lighting, and music. It can even be used to power electric vehicle charging solutions such as the new ABB AC wallbox, and activate new smart functionalities based on energy information.

For areas with unreliable power supplies, REACT 2 also offers a backup function to guarantee power in case of blackout.

ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in electrification products, robotics and motion, industrial automation and power grids, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner of Formula E, the fully electric international FIA motorsport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 135,000 employees. www.abb.com

-
For more information please contact:

Natalie Hodges

ABB Ltd
Media Relations Manager Affolternstrasse 44
Electrification Products Division
Phone: +41 (0)43 317 54 04
E-mail: natalie.hodges@ch.abb.com
8050 Zurich
Switzerland

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp