ABB retraces its pioneering technology roots to upgrade world’s first HVDC link

The high-voltage direct current (HVDC) transmission line between mainland Sweden and the island of Gotland was originally installed by ABB and will now be upgraded. The latest step for this ground-breaking technology will enable more renewable energy integration and boost the island’s grid reliability.

The world's first commercial HVDC transmission system came into operation in 1954. Installed by ABB, it was a technological milestone in the company's 125-year history, just one example of how ABB's innovations help shape the future. ABB continues to be a market and technology leader in this space and today, amongst its increasing number of applications, HVDC is playing a key role in integrating renewables, evacuating power efficiently and reliably across long distances and interconnecting regions and countries.

Gotland again witnessed history when, in 1999, the world's first interconnection using HVDC Voltage Sourced Converter (VSC) technology, called HVDC Light by ABB, was installed on the island. The HVDC installation has been progressively upgraded by ABB as this technology has developed, and ABB has now won orders from Vattenfall Eldistribution AB for this latest upgrade, taking the company back to the roots of the technology it pioneered.

The 150-kilovolt (kV) link has the capacity to transmit 320 megawatts (MW) of power 100 kilometers from Västervik, on the east coast of mainland Sweden, to Ygne, on the island of Gotland. The link provides electricity to meet the needs of the 58,000 residents of Gotland and enables wind power, generated on the island, to be transmitted to the mainland. This upgrade will help enhance capacity and enable a greater amount of wind power generation on Gotland, to be integrated into the grid for use both locally in Sweden and across borders.

As a key element of the upgrade ABB will install its state-of-the-art MACH control and protection system, which is like the brain of an HVDC link. ABB's MACH control system offers unmatched calculation capacity and a high degree of integration capability to handle control and protection functions, designed to run around the clock for 30 years or more. It also incorporates advanced fault registration and remote control functions. The cooling system will also be upgraded as part of the project. The upgrades replace aging equipment and will help improve security of power supply to the island. The addition of a modern operator interface will also help extend the lifetime of the link in addition to providing improved availability and functionality.

"Having pioneered HVDC technology by commissioning this first commercial link in 1954, we are proud to provide a new life to this critical asset. By enabling more wind power integration more people will benefit from clean renewable energy, helping to lower environmental impact," said Patrick Fragman, Managing Director of ABB's Grid Systems business, part of the company's Power Grids division. "This upgrade project reaffirms our Next Level strategy focus on providing our customers with differentiated value through technology, during the whole life cycle of build-up, operation and maintenance of their assets."

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp